Grove - Finger-clip Heart Rate Sensor

Grove - Finger-clip Heart Rate Sensor is based on PAH8001EI-2G, a high performance and low power CMOS-process optical sensor with Green LED and DSP integrated serving as a Heart Rate Detection(HRD) sensor. This module is based on optical technology which measures the variation human blood movement in the vessel. Low power consumption and flexible power saving mode make it suitable for wearable device. Cause the heart rate sensor chip need high processing speed for the algorithm of heart rate data(), this module integrate a STM32, reserved SWD interface allow users to reprogram the STM32.
Specification
-
Ultra-low power consumption, power saving mode during time of no touch movement
-
Flexible sleep rate control
-
Integrated the STM32F103
-
I2C interface
-
Heart rate sensor area just 3.0 x 4.7mm
-
Reserved SWD interface
-
Working temperature: -20 ~ +60℃
Interface Function


-
1: Grove Interface
-
2: Reserved SWD Interface for programming to STM32
-
3: Heart Rate Sensor
Usage
Here, We will provide an example here to show you how to use this sensor.
Hardware Installation
Link the Sensor to I2C port of Seeeduino with Grove Cable.

Software Part
With Arduino
Hardware Serial
Copy the following code into a new sketch of Arduino and upload the sketch, then you can get heart rate from the Serial Monitor. It may take about a minute to get valid heart rate after you touch your finger with sensor.
#include <Wire.h>
void setup() {
Serial.begin(9600);
Serial.println("heart rate sensor:");
Wire.begin();
}
void loop() {
Wire.requestFrom(0xA0 >> 1, 1); // request 1 bytes from slave device
while(Wire.available()) { // slave may send less than requested
unsigned char c = Wire.read(); // receive heart rate value (a byte)
Serial.println(c, DEC); // print heart rate value
}
delay(500);
}
Software Serial
The standard I2C library for the Arduino is the Wire Library. While this library does not work when the I2C pins SDA/SCL are in use already for other purposes. So you can use the SoftwareI2C. You can connect the SCL to D2 and SDA to D3. Please download the SoftI2CMaster library and follow How to install arduino library to setup the library. Copy the following code into a new sketch of Arduino and upload the sketch, then you can get heart rate from the Serial Monitor. It may take about a minute to get valid heart rate after you touch your finger with sensor.
#define SDA_PORT PORTD
#define SDA_PIN 3
#define SCL_PORT PORTD
#define SCL_PIN 2
#include <SoftI2CMaster.h>
#include <SoftWire.h>
SoftWire Wire = SoftWire();
void setup() {
Serial.begin(9600);
Serial.println("heart rate sensor:");
Wire.begin();
}
void loop() {
Wire.requestFrom(0xA0 >> 1, 1); // request 1 bytes from slave device
while(Wire.available()) { // slave may send less than requested
unsigned char c = Wire.read(); // receive heart rate value (a byte)
Serial.println(c, DEC); // print heart rate value
}
delay(500);
}
With Mbed
Read a byte from I2C device 0xA0 (8 bit address), it's the heart rate.
#include "mbed.h"
I2C i2c(I2C_SDA, I2C_SCL);
const int addr = 0xA0;
int main() {
char heart_rate;
while (1) {
i2c.read(addr, &heart_rate, 1);
printf("heart rate: = %d\r\n", heart_rate);
}
}
Upgrade firmware
We can upgrade the firmware of the heart rate sensor through its bootloader.
- The bootloader is located at 0x08000000 - 0x08002000
- The application is located at 0x08002000 - 0x08020000
Hardware Connection

- USB to serial adapter is required
- UART (the Grove connector supports I2C and UART),when upgrade the firmware, the Grove interface run in UART mode.
| Grove-Finger-clip_Heart_Rate_Sensor | USB to Serial (TTL) Module&Adapter |
|---|---|
| VCC | VCC |
| GND | GND |
| SDA | TX |
| SCL | RX |
Software
- Download Tera Term Software
- Set UART Baud Rate as 115200

-
Download firmware
-
Select Grove - Finger-clip Heart Rate Sensor.bin

- Downloading the firmware to Grove-Finger-clip_Heart_Rate_Sensor

- Firmware download successfully

Grove - Finger-clip Heart Rate Sensor provide heart rate measurements.However, it is not a medical device. To use the heart rate detection sensor on your wrist, finger or palm, you must:
-
Fasten the sensor snugly makes tight contact with your skin and maintain table (no motion) while measuring to acquire accurate heart rate.If the sensor does not contact the skin well or have extreme motion while measuring that the heart rate will not be measured correctly.
-
Sensor's performance is optimized with greater blood flow. On cold days or users have poor circulation(ex: cold hands, fingers and cold feet) the sensor performance (heart rate accuracy) can be impacted because of lower blood flow in the measuring position.
Schematic Online Viewer
Resource
Tech Support & Product Discussion
Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.