Skip to main content

Grove Port

This repo introduces how to use Wio Terminal with the Grove Ecosystem.

With the help of Grove, you are able prototype much quicker with simpler connections!

Wio Terminal With Grove - TDS Sensor

This section introduces how to use Grove - TDS Sensor with Wio Terminal to display real time TDS readings on a line chart!

Libraries Installation

  1. Install the LCD library.

  2. Install the Linechart library.

Complete Code

Connect the Grove TDS sensor to the Grove D/A Pin of Wio Terminal, upload the code and check the results!

#include"seeed_line_chart.h" //include the library
TFT_eSPI tft;

#define max_size 50 //maximum size of data
doubles data; //Initilising a doubles type to store data
TFT_eSprite spr = TFT_eSprite(&tft); // Sprite

#define sensorPin A0 //Analog pin

int sensorValue = 0;
float tdsValue = 0;
float Voltage = 0;

void setup() {
pinMode(sensorPin, INPUT);
tft.begin();
tft.setRotation(3);
spr.createSprite(TFT_HEIGHT,TFT_WIDTH);
}

void loop() {
spr.fillSprite(TFT_WHITE);

sensorValue = analogRead(sensorPin);
Voltage = sensorValue*5/1024.0; //Convert analog reading to Voltage
tdsValue=(133.42*Voltage*Voltage*Voltage - 255.86*Voltage*Voltage + 857.39*Voltage)*0.5; //Convert voltage value to TDS value

if (data.size() == max_size) {
data.pop();//this is used to remove the first read variable
}
data.push(tdsValue); //read variables and store in data

//Settings for the line graph title
auto header = text(0, 0)
.value("TDS Reading")
.align(center)
.valign(vcenter)
.width(tft.width())
.thickness(3);

header.height(header.font_height() * 2);
header.draw(); //Header height is the twice the height of the font

//Settings for the line graph
auto content = line_chart(20, header.height()); //(x,y) where the line graph begins
content
.height(tft.height() - header.height() * 1.5) //actual height of the line chart
.width(tft.width() - content.x() * 2) //actual width of the line chart
.based_on(0.0) //Starting point of y-axis, must be a float
.show_circle(true) //drawing a cirle at each point, default is on.
.value(data) //passing through the data to line graph
.color(TFT_RED) //Setting the color for the line
.draw();

spr.pushSprite(0, 0);
delay(50);
}

Wio Terminal With Grove - OLED Display

If you required a second screen to display with Wio Terminal, Grove - OLED Dispaly 0.96" will be the perfect choice. It can be used to display graphics and data, adding more interactive features with Wio Terminal.

Libraries Installation

  1. Install the U8g2 libraries from the Library Manager in Arduino IDE. Navigate to Sketch -> Include Library -> Manage Libraries... and Search and install U8g2 in the Library Manager.

U8g2 Initilization

Initialuse the OLED display using u8g2's software I2C and use SCL for clock and SDA for Data:

U8G2_SSD1306_128X64_NONAME_1_SW_I2C u8g2(U8G2_R0, /* clock=*/ SCL, /* data=*/ SDA, /* reset=*/ U8X8_PIN_NONE);

Usage

  1. Call u8g2.firstPage().

  2. Start a do-while loop.

  3. Inside the loop-body: Draw something with the usual draw commands.

  4. Loop as long as u8g2.nextPage() returns true.

For more information, please visit u8g2

Complete Code

Connect the Grove OLED Display 0.96" to the Grove I2C pin and check the results!

#include <U8g2lib.h>

U8G2_SSD1306_128X64_NONAME_1_SW_I2C u8g2(U8G2_R0, /* clock=*/ SCL, /* data=*/ SDA, /* reset=*/ U8X8_PIN_NONE);

const unsigned char WAVE[] PROGMEM = {
0x00,0x00,0x00,0x00,0x00,0x00,0x00,
0x00,0x00,0x00,0x00,0x00,0x00,0x00,
0x00,0x00,0x00,0x00,0x00,0x00,0x00,
0x00,0x00,0x00,0x00,0x00,0x00,0x00,
0x00,0x00,0x00,0x00,0x00,0x00,0x00,
0x00,0x00,0x00,0x00,0x00,0x00,0x00,
0x00,0x00,0x00,0x00,0x00,0x00,0x00,
0x00,0x00,0x00,0x00,0x00,0x00,0x00,
0x00,0x00,0x00,0x00,0x00,0x00,0x00,
0xF0,0x00,0xFF,0x00,0x0F,0xF0,0x00,
0xFC,0x03,0xFF,0xC0,0x3F,0xFC,0x00,
0xFE,0x07,0xFF,0xE0,0x7F,0xFE,0x00,
0x1F,0xFF,0x81,0xFF,0xF8,0x1F,0xC0,
0x0F,0xFF,0x00,0xFF,0xF0,0x0F,0xC0,
0x03,0xFC,0x00,0x3F,0xC0,0x03,0xC0,
0x00,0x00,0x00,0x00,0x00,0x00,0x00,
0x00,0x00,0x00,0x00,0x00,0x00,0x00,
0xE0,0x00,0x7E,0x00,0x07,0xE0,0x00,
0xF8,0x01,0xFF,0x80,0x1F,0xF8,0x00,
0xFC,0x03,0xFF,0xC0,0x3F,0xFC,0x00,
0xFF,0x0F,0xFF,0xF0,0xFF,0xFF,0x00,
0x1F,0xFF,0x81,0xFF,0xF8,0x1F,0xC0,
0x07,0xFE,0x00,0x7F,0xE0,0x07,0xC0,
0x01,0xF8,0x00,0x1F,0x80,0x01,0xC0,
0x00,0x00,0x00,0x00,0x00,0x00,0x00,
0x00,0x00,0x00,0x00,0x00,0x00,0x00,
0xF0,0x00,0xFF,0x00,0x0F,0xF0,0x00,
0xF8,0x01,0xFF,0x80,0x1F,0xF8,0x00,
0xFE,0x07,0xFF,0xE0,0x7F,0xFE,0x00,
0x3F,0xFF,0xC3,0xFF,0xFC,0x3F,0xC0,
0x0F,0xFF,0x00,0xFF,0xF0,0x0F,0xC0,
0x07,0xFE,0x00,0x7F,0xE0,0x07,0xC0,
0x00,0xF0,0x00,0x0F,0x00,0x00,0xC0,
0x00,0x00,0x00,0x00,0x00,0x00,0x00,
0x80,0x00,0x18,0x00,0x01,0x80,0x00,
0xF0,0x00,0xFF,0x00,0x0F,0xF0,0x00,
0xFC,0x03,0xFF,0xC0,0x3F,0xFC,0x00,
0xFF,0x0F,0xFF,0xF0,0xFF,0xFF,0x00,
0x1F,0xFF,0x81,0xFF,0xF8,0x1F,0xC0,
0x0F,0xFF,0x00,0xFF,0xF0,0x0F,0xC0,
0x03,0xFC,0x00,0x3F,0xC0,0x03,0xC0,
0x00,0x00,0x00,0x00,0x00,0x00,0x00,
0x00,0x00,0x00,0x00,0x00,0x00,0x00,
0x00,0x00,0x00,0x00,0x00,0x00,0x00,
0x00,0x00,0x00,0x00,0x00,0x00,0x00,
0x00,0x00,0x00,0x00,0x00,0x00,0x00,
0x00,0x00,0x00,0x00,0x00,0x00,0x00,
0x00,0x00,0x00,0x00,0x00,0x00,0x00,
0x00,0x00,0x00,0x00,0x00,0x00,0x00,
0x00,0x00,0x00,0x00,0x00,0x00,0x00
};

void setup() {
u8g2.begin();
}

void loop() {
u8g2.firstPage();
do {
u8g2.setFont(u8g2_font_t0_16b_mr);
u8g2.drawXBMP(40, 0, 50, 50, WAVE);
u8g2.setCursor(20, 60);
u8g2.print("Wio Terminal");
} while (u8g2.nextPage());
}

Wio Terminal With Grove - Temperature Sensor

This section introduces how to use Grove - Temperature Sensor with Wio Terminal to display real-time surrounding temperature readings.

Libraries Installation

  1. Install the LCD library.

  2. Install the Linechart library.

Complete Code

Connect the Grove Temperature sensor to the Grove D/A Pin of Wio Terminal, upload the code and check the results!

#include"seeed_line_chart.h" //include the library
#include <math.h>

TFT_eSPI tft;

#define max_size 50 //maximum size of data
doubles data; //Initilising a doubles type to store data
TFT_eSprite spr = TFT_eSprite(&tft); // Sprite

const int B = 4275; // B value of the thermistor
const int R0 = 100000; // R0 = 100k
const int pinTempSensor = A0; // Grove - Temperature Sensor connect to A0

void setup() {
pinMode(pinTempSensor, INPUT);
tft.begin();
tft.setRotation(3);
spr.createSprite(TFT_HEIGHT,TFT_WIDTH);
}

void loop() {
spr.fillSprite(TFT_DARKCYAN);

int a = analogRead(pinTempSensor);
float R = 1023.0/a-1.0;
R = R0*R;

float temperature = 1.0/(log(R/R0)/B+1/298.15)-273.15; // convert to temperature via datasheet

if (data.size() == max_size) {
data.pop();//this is used to remove the first read variable
}
data.push(temperature); //read variables and store in data

//Settings for the line graph title
auto header = text(0, 0)
.value("Temperature Reading")
.align(center)
.color(TFT_WHITE)
.valign(vcenter)
.width(tft.width())
.thickness(2);

header.height(header.font_height() * 2);
header.draw(); //Header height is the twice the height of the font

//Settings for the line graph
auto content = line_chart(20, header.height()); //(x,y) where the line graph begins
content
.height(tft.height() - header.height() * 1.5) //actual height of the line chart
.width(tft.width() - content.x() * 2) //actual width of the line chart
.based_on(0.0) //Starting point of y-axis, must be a float
.show_circle(true) //drawing a cirle at each point, default is on.
.y_role_color(TFT_WHITE)
.x_role_color(TFT_WHITE)
.value(data) //passing through the data to line graph
.color(TFT_RED) //Setting the color for the line
.draw();

spr.pushSprite(0, 0);
delay(50);
}

Wio Terminal With Grove - GPS Sensor

This section introduces how to use Grove - GPS Sensor with Wio Terminal for obtaining real-time GPS information. The sensor itself outputs NMEA GPS data which we will use the TinyGPSPlus library to parse the data to readable information.

Libraries Installation

  1. Install the TinyGPSPlus Library.

Complete Code

Connect the Grove GPS Sensor to the Grove I2C Pin (Left Side) of Wio Terminal, upload the code and check the results in Serial Monitor(w/ baud rate: 9600)!

#include <TinyGPS++.h>
#include <wiring_private.h>

static const uint32_t GPSBaud = 9600;

// The TinyGPS++ object
TinyGPSPlus gps;

// The serial connection to the GPS device - Left side Grove connector.
// Left side Grove connector shares pins with I2C1 of 40 pin connector.
static Uart Serial3(&sercom3, PIN_WIRE_SCL, PIN_WIRE_SDA, SERCOM_RX_PAD_1, UART_TX_PAD_0);

void setup()
{
Serial.begin(115200);

Serial3.begin(GPSBaud);
pinPeripheral(PIN_WIRE_SCL, PIO_SERCOM_ALT);
pinPeripheral(PIN_WIRE_SCL, PIO_SERCOM_ALT);
}

void loop()
{
// This sketch displays information every time a new sentence is correctly encoded.
while (Serial3.available() > 0)
if (gps.encode(Serial3.read()))
displayInfo();

if (millis() > 5000 && gps.charsProcessed() < 10)
{
Serial.println(F("No GPS detected: check wiring."));
while(true);
}
}

void displayInfo()
{
Serial.print(F("Location: "));
if (gps.location.isValid())
{
Serial.print(gps.location.lat(), 6);
Serial.print(F(","));
Serial.print(gps.location.lng(), 6);
}
else
{
Serial.print(F("INVALID"));
}

Serial.print(F(" Date/Time: "));
if (gps.date.isValid())
{
Serial.print(gps.date.month());
Serial.print(F("/"));
Serial.print(gps.date.day());
Serial.print(F("/"));
Serial.print(gps.date.year());
}
else
{
Serial.print(F("INVALID"));
}

Serial.print(F(" "));
if (gps.time.isValid())
{
if (gps.time.hour() < 10) Serial.print(F("0"));
Serial.print(gps.time.hour());
Serial.print(F(":"));
if (gps.time.minute() < 10) Serial.print(F("0"));
Serial.print(gps.time.minute());
Serial.print(F(":"));
if (gps.time.second() < 10) Serial.print(F("0"));
Serial.print(gps.time.second());
Serial.print(F("."));
if (gps.time.centisecond() < 10) Serial.print(F("0"));
Serial.print(gps.time.centisecond());
}
else
{
Serial.print(F("INVALID"));
}

Serial.println();
}

void SERCOM3_0_Handler()
{
Serial3.IrqHandler();
}
void SERCOM3_1_Handler()
{
Serial3.IrqHandler();
}
void SERCOM3_2_Handler()
{
Serial3.IrqHandler();
}
void SERCOM3_3_Handler()
{
Serial3.IrqHandler();
}
Loading Comments...