Overview
This repo introduce how to install the TFT LCD library used on Wio Terminal. It provides basic graphical functions to the Wio Terminal with minimum effort!
TFT LCD Library Default Installation
By default, the TFT LCD Library is included inside the Wio Terminal Board Library. Hence, there is no need to download the TFT LCD library again. Follow the next tutorials to get you started with the display!
Installing the TFT LCD Library Separately
If you want to install the TFT LCD library separately, or updating just the TFT LCD library, follow the steps below:
Visit the Seeed_Arduino_LCD repositories and download the entire repo to your local drive.
Now, the TFT LCD library can be installed to the Arduino IDE. Open the Arduino IDE, and click
sketch
->Include Library
->Add .ZIP Library
, and choose theSeeed_Arduino_LCD
file that you've have just downloaded.
Installing the Adafruit Zero DMA Library
Some functions of the TFT LCD Library requires this library.
Navigate to
sketch
->Include Library
->Manager Library
, and a library manager window will appear.Search Adafruit Zero DMA and click Install.
Tech Support & Product Discussion
if you have any technical issue. submit the issue into our forum. Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.