Skip to main content

Grove Base Shield for Photon

Features


  • Grove interfaced

  • Connect to massive and low-cost Grove modules

  • I2C, UART ports integrated

Application ideas


  • Compact IoT applications such as smart router.

Specification


Grove ports 3 digital ports

2 analog ports

2 I2C ports

1 UART port.

Dimensions 53 × 53 mm
Weight 18g

Hardware Overview


Parts list

Parts name Quantity
Grove Base Shield for Photon 1PC

Getting Started


Note: In this case we show you a general development environmental.

Buzzing

1. Refer to [here](https://docs.particle.io/guide/getting-started/connect/core/) to connect to a device (PC or Mac).

!!!Note

1. We recommend that you choose **node.js v4.2.3 LTS** especially for Windows 10 user.
2. You may need to one more steps after run command **particle setup**, that is, connect you device (PC or Mac) to a wi-fi AP whose name contain **Photon**, especially on Windows 10.
2. Use [Web IDE](https://build.particle.io/) for your project. Login with your account and choose your device (click the 2nd last icon on left column).
note
We recommend you choose [Web IDE](https://build.particle.io/) to compile or flashing your code to Photon which is much quicker than using Particle Dev, if your internet connectivity is not so good.
3. Connect them like following:

4. Now you can copy following code to Web IDE and flash them to Photo by clicking a lighting-like icon (the 1st icon on left column).
note
Copy the code only to the tab named _**filename.ino**_.
/*
Buzzing
Use digital pin D4
This example code is in the public domain.
by xiaohe
*/
int led1 = D4; //set D4 as output

void setup() {
pinMode(led1, OUTPUT);
}

void loop() {
// enable buzzing
digitalWrite(led1, HIGH);

// We'll leave it on for 1 second...
delay(1000);

// Then we'll turn it off...
digitalWrite(led1, LOW);

// Wait 1 second...
delay(1000);

// And it will repeat!
}

Schematic Online Viewer

Resources


Tech Support & Product Discussion

Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.

Loading Comments...