Skip to main content

Grove - NOT


This Grove module provides the function of a logical NOT gate. It is based on the 74HC1G04GW chip. The 74HC1G04GW is a high-speed Si-gate CMOS device that provides the inverting buffer. The NOT module has one input on the left and one output on the right. When the input signal is HIGH, output signal is LOW. When the input signal is LOW, output signal is HIGH.

Features

  • Simple NOT gate function with one input and one output

  • Makes integrating a Logical NOT in your circuit a breeze

  • Uses Standard 4-pin Grove Cables to connect to other Grove modules

Usage

  • See the Glow-in-the-dark LED String Lights example on the Grove Mixer Pack V2 wiki page for how to build a circuit that uses NOT Logic.

  • Also see Grove - NOT module typical usage

See also

  • Grove - OR

  • Grove - AND

Availability

This Grove module is available as part of the following Grove Kit Series:

  • Grove Mixer Pack V2

Note that this Grove - NOT module is sold only as part of the above mentioned packs and is not available stand-alone from the Seeed Studio Bazaar.

Schematic Online Viewer

Resources

Tech Support & Product Discussion

Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.

Loading Comments...