edit

Seeeduino Ethernet

Seeeduino Ethernet is a compact and multifunctional development platform, which merges data logging and processing, device control and Ethernet communication together into one. It's armed with a MEGA328P chip and a Wiz5100: the former provides an Arduino controlling style and the latter provides TCP and UDP Ethernet communication ability. Plus integrated SD card module, it's convenient and neat for remote data logging, processing or transferring via network.

In this version, we lowered the height of RJ45 to balance it with the headers. Besides, with an I2C and a UART Grove port populated,it's convenient to connect corresponding Grove modules to this board.

Specification


  • Voltage: 6.2-13V

  • Current: 140-550mA

  • Supported Card Type: Micro SD card(must be SanDisk), FAT/FAT32 (More than 2G is not guaranteed)

  • Supported Connection: TCP/UDP

  • Net Weight: 23±2g *

  • Ethernet jack: Standard RJ45

Demonstration


We will test the Seeeduino Ethernet functions of writing or reading information from the SD Card and sending out A/D data to network.

Step 1: Install the Hardware

Firstly, install the hardware. We have two alternatives to plug in the power.

Method 1: You can use one Passive PoE Cable Set to provide power and Ethernet connection at the same time like the picture below.

Method 2: Use separate power cable and Ethernet cable.

Step 2: Programing

After hardware installation, here we continue to try the test code. This program is written to test the functions of writing or reading data from the SD Card and sending out A/D data to network. This demo code can be used as a test program as well as reference if you wanna explore more functions of the board.

NOTICE:

  1. All the ".h" file needed have been pre-installed in Arduino IDE(1.0).

  2. Install a Micro SD card. Make sure the Micro SD card is not full and the format is FAT or FAT32.

      1
      2
      3
      4
      5
      6
      7
      8
      9
     10
     11
     12
     13
     14
     15
     16
     17
     18
     19
     20
     21
     22
     23
     24
     25
     26
     27
     28
     29
     30
     31
     32
     33
     34
     35
     36
     37
     38
     39
     40
     41
     42
     43
     44
     45
     46
     47
     48
     49
     50
     51
     52
     53
     54
     55
     56
     57
     58
     59
     60
     61
     62
     63
     64
     65
     66
     67
     68
     69
     70
     71
     72
     73
     74
     75
     76
     77
     78
     79
     80
     81
     82
     83
     84
     85
     86
     87
     88
     89
     90
     91
     92
     93
     94
     95
     96
     97
     98
     99
    100
    101
    102
    103
    104
    105
    106
    107
    108
    109
    110
    111
    112
    113
    114
    115
    116
    117
    118
    119
    120
    121
    122
    123
    124
    125
    126
    127
    128
    129
    130
    131
    132
    133
    134
    135
    136
    137
    138
    139
    140
    141
    142
    143
    144
    145
    146
    147
    148
    149
    150
    151
    152
    153
    154
    155
    156
    157
    158
    159
    160
    161
    162
    163
    164
    165
    166
    167
    168
    169
    170
    171
    172
    /*
      SD card read/write
    
     This example shows how to read and write data to and from an SD card file
     The circuit:
     * SD card attached to SPI bus as follows:
     ** MOSI - pin 11
     ** MISO - pin 12
     ** CLK - pin 13
     ** CS - pin 4
    
       Web Server
    
     A simple web server that shows the value of the analog input pins.
     using an Arduino Wiznet Ethernet shield.
    
     Circuit:
     * Ethernet shield attached to pins 10, 11, 12, 13
     * Analog inputs attached to pins A0 through A5 (optional)
    
     created 18 Dec 2009
     by David A. Mellis
     modified 4 Sep 2010
     by Tom Igoe
    
     */
    
    #include <SD.h>
    #include <SPI.h>
    #include <Ethernet.h>
    
    // Enter a MAC address and IP address for your controller below.
    // The IP address will be dependent on your local network:
    byte mac[] = { 0xDE, 0xAD, 0xBE, 0xEF, 0xFE, 0xED };
    IPAddress ip(192,168,1,177);
    
    // Initialize the Ethernet server library
    // with the IP address and port you want to use
    // (port 80 is default for HTTP):
    EthernetServer server(80);
    
    File myFile;
    
    void setup()
    {
        Serial.begin(9600);
        Serial.print("Initializing SD card...");
        // On the Ethernet Shield, CS is pin 4. It's set as an output by default.
        // Note that even if it's not used as the CS pin, the hardware SS pin
        // (10 on most Arduino boards, 53 on the Mega) must be left as an output
        // or the SD library functions will not work.
        pinMode(10, OUTPUT);
        // pinMode(4,OUTPUT);
        if (!SD.begin(4)) {
            Serial.println("initialization failed!");
            return;
        }
        Serial.println("initialization done.");
    
        // open the file. note that only one file can be open at a time,
        // so you have to close this one before opening another.
    
        myFile = SD.open("test.txt",FILE_WRITE);
        // if the file opened or created okay, write to it:
        if (myFile) {
            Serial.print("Writing to test.txt...");
            myFile.println("testing 1, 2, 3.");
            // close the file:
            myFile.close();
            Serial.println("done.");
        } else {
            // if the file didn't open, print an error:
            Serial.println("error opening test.txt");
        }
    
        // re-open the file for reading:
        myFile = SD.open("test.txt");
        if (myFile) {
            Serial.println("test.txt:");
    
            // read from the file until there's nothing else in it:
            while (myFile.available()) {
                Serial.write(myFile.read());
            }
            // close the file:
            myFile.close();
        } else {
            // if the file didn't open, print an error:
            Serial.println("error opening test.txt");
        }
        // start the Ethernet connection and the server:
        Ethernet.begin(mac, ip);
        server.begin();
    }
    unsigned char buff[6];
    void loop()
    {
        EthernetClient client = server.available();
        if (client) {
            // an http request ends with a blank line
            boolean currentLineIsBlank = true;
            while (client.connected()) {
                if (client.available()) {
                    char c = client.read();
                    // if you've gotten to the end of the line (received a newline
                    // character) and the line is blank, the http request has ended,
                    // so you can send a reply
                    if (c == '\n' && currentLineIsBlank) {
                        // send a standard http response header
                        client.println("HTTP/1.1 200 OK");
                        client.println("Content-Type: text/html");
                        client.println();
    
                        // output the value of each analog input pin
                        for (int analogChannel = 0; analogChannel < 6; analogChannel++) {
                            client.print("analog input ");
                            client.print(analogChannel);
                            client.print(" is ");
                            client.print(analogRead(analogChannel));
                            client.println("<br />");
                            buff[analogChannel] = analogRead(analogChannel);
                        }
                        break;
                    }
                    if (c == '\n') {
                        // you're starting a new line
                        currentLineIsBlank = true;
                    }
                    else if (c != '\r') {
                        // you've gotten a character on the current line
                        currentLineIsBlank = false;
                    }
                }
            }
            // give the web browser time to receive the data
            delay(1);
            // close the connection:
            client.stop();
            myFile = SD.open("test.txt", FILE_WRITE);
            if (myFile) {
                Serial.println("test.txt:");
                for (int analogChannel = 0; analogChannel < 6; analogChannel++) {
                    myFile.print("analog input ");
                    myFile.print(analogChannel);
                    myFile.print(" is ");
                    myFile.println(analogRead(analogChannel));
                }
                // read from the file until there's nothing else in it:
                myFile.close();
            }
            else {
                // if the file didn't open, print an error:
                Serial.println("error opening test.txt");
            }
    
            myFile = SD.open("test.txt");
            if (myFile) {
                Serial.println("test.txt:");
    
                // read from the file until there's nothing else in it:
                while (myFile.available()) {
                    Serial.write(myFile.read());
                }
                // close the file:
                myFile.close();
            }
            else {
                // if the file didn't open, print an error:
                Serial.println("error opening test.txt");
            }
        }
    }
    

Step 3: Download the program

Because there is no USB connector on the board. Seeeduino Ethernet requires a UartSBee to download the program.

Connect the UartSBee to Seeeduino Ethernet as below:

Warning

Please select Seeeduino V3.0 as board in tool menu to download the program.

Step 4: Result testing

NOTICE: Make sure the Seeeduino Ethernet and your computer are in the same local area network. After the program was downloaded, open the Serial Monitor. You will check the status of the board.

Open a web browser and enter the web address:192.168.1.177, then you can check the data sent out by Seeeduino Ethernet:

Schematic Online Viewer

Resources

Tech Support

Please submit any technical issue into our forum.