edit

Motor Shield‏‎

The Motor Shield is a driver module for motors that allows you to use Arduino to control the working speed and direction of the motor

Motor Shield V1.0 Motor Shield V2.0

Here lists the comparison between various versions of Motor Shield:

Parameter Motor Shield V1.0 Motor Shield V2.0
Working Voltage +5V +5V
Power Extern power supply Extern power or +5 Pin of Arduino/Seeeduino

Tech Support

Please do not hesitate to contact techsupport@seeed.cc if you have any technical issue. Or submit the issue into our forum.