Skip to main content

Weekly Wiki ✨

Greetings

This is Matthew in Seeed Studio and welcome to the Seeed Studio weekly wiki! Each Monday, I will introduce you our latest wiki, including the ones related to our new products, the interesting projects published by Seeed Studio, and the tutorials, introductions, etc... You name it.

✨ For each week, when a collaborator contributes a project or fixes something important, we put the stars at the end of title of "Weekly Wiki" for more people be able to see their efforts👍.

Today is September 3rd and a brand new week has begun! Check out what Seeed Studio did last week!

Latest Wiki Launched

mmWave Human Detection Sensor Kit

Introducing our ready-to-use, open-source mmWave Human Detection Sensor Kit, driven by the Seeed Studio XIAO ESP32C3. This kit comes with an onboard 24GHz mmWave Human Static Presence Module Lite, which can be swapped out for any mmWave series sensor from Seeed. Additionally, we've provided two reserved Grove interfaces (Analog, IIC) that enable connectivity with over 400 different Grove modules, expanding the kit's capabilities extensively.

SenseCAP M2 Multi-Platform Gateway LNS Configuration

We have added LNS Configuration for SenseCAP M2 Multi-Platform Gateway.

Existed Wiki Updated

SenseCAP T1000 Tranker Ubidots Decoder

We have upgraded the devoder for Ubidots.

The Efforts of Contributor✨

Micropython for XIAO ESP32S3 Sense(Camera, Wi-Fi)

The firmware designed for XIAO ESP32S3 Sense is made by our friend, shariltumin whom we are really greatful for. And thanks Hendra for testing it, thinking full-featured and writing us a wiki!

SenseCAP Indicator x Matter Application Development

Thanks our contributor Tim for establishing a demo of how to use the Matter SDK to build enriched applications for the SenseCAP Indicator.

Reorgizing the wiki of Grove - Wio-e5 uploading the data and adding a new one as uploading data to Helium Cloud

Thanks our contributor Salman for reorganizing the wiki of Grove - Wio-e5 uploading the data and adding a new wiki: Uploading data to Helium Cloud using Seeed Studio XIAO SAMD21.

Past Weekly wiki

Loading Comments...