Grove - Serial MP3 Player
Grove-Serial MP3 Player is a kind of simple MP3 player device whose design is based on a high-quality MP3 audio chip---WT5001. It can support 8KHZ~44.1kHZ sampling frequency MP3 and WAV file formats. This product has several peripheral ports: a standard UART Grove interface, a dual track headphone jack, an external interface and also a Micro SD card interface. You can control the MP3 playback state by sending commands to module via serial port tools, such as switch songs, change the volume and play mode and so on. It seems a simple module, but it owns such strong function. Want to know how the sound quality is? Please come and experience it!
Features¶
- Standard Grove interface
- Asynchronous serial port control play mode
- Busy Indicator
- Reset Button
- Standard Micro SD card Interface
- Support FAT16 and FAT32 file system
Tip
More details about Grove modules please refer to Grove System
Platforms Supported¶
Arduino | Raspberry Pi | BeagleBone | Wio | LinkIt ONE |
---|---|---|---|---|
![]() |
![]() |
![]() |
![]() |
![]() |
Caution
The platforms mentioned above as supported is/are an indication of the module's hardware or theoritical compatibility. We only provide software library or code examples for Arduino platform in most cases. It is not possible to provide software library / demo code for all possible MCU platforms. Hence, users have to write their own software library.
Hardware Overview¶
- ①:Left Channel Grove Interface.
- ②:Headset Interface:3.5mm headphones
- ③:Right Channel Grove Interface.
- ④:WT5001
- ⑤:LED Indicator:LED is on when music is playing.
- ⑥:UART Grove Interface
- ⑦:SD Card: micro SD Card(≤2GB)
Usage¶
The Grove - Serial MP3 Play can be controlled by Arduino/Seeeduino. And there is a Serial_MP3 test code for you to use. I believe you can easily get started. For more detailed information, please refer to the following description. The hardware installation:
- Connect Grove - Serial MP3 Play to the Digital 2 port of Arduino/Seeeduino, Notice that you can change the pin number as you like, just make sure corresponding changes the code. Then connect your Arduino/Seeeduino to PC with a USB cable.
- Plug a earphone into Grove - Serial MP3 Play. Now the hardware part has been completed.
- After uploading it, open serial tool to send commands.
- Upload the code below.
The following code includes play mode parameter. You only need to change the parameter to switch the play mode.
/*****************************************************************************/ // Function: control the seeedstudio Grove MP3 player // Hardware: Grove - Serial MP3 Player /*******************************************************************************/ #include <SoftwareSerial.h> SoftwareSerial mp3(2, 3);//modify this with the connector you are using. void setup() { mp3.begin(9600); Serial.begin(9600); delay(100); if (true ==SetPlayMode(0x01)) Serial.println("Set The Play Mode to 0x01, Single Loop Mode."); else Serial.println("Playmode Set Error"); PauseOnOffCurrentMusic(); } void loop() { SetPlayMode(0x01); delay(1000); SetMusicPlay(00,01); delay(1000); SetVolume(0x0E); while(1); } //Set the music index to play, the index is decided by the input sequence //of the music; //hbyte: the high byte of the index; //lbyte: the low byte of the index; boolean SetMusicPlay(uint8_t hbyte,uint8_t lbyte) { mp3.write(0x7E); mp3.write(0x04); mp3.write(0xA0); mp3.write(hbyte); mp3.write(lbyte); mp3.write(0x7E); delay(10); while(mp3.available()) { if (0xA0==mp3.read()) return true; else return false; } } // Pause on/off the current music boolean PauseOnOffCurrentMusic(void) { mp3.write(0x7E); mp3.write(0x02); mp3.write(0xA3); mp3.write(0x7E); delay(10); while(mp3.available()) { if (0xA3==mp3.read()) return true; else return false; } } //Set the volume, the range is 0x00 to 0x1F boolean SetVolume(uint8_t volume) { mp3.write(0x7E); mp3.write(0x03); mp3.write(0xA7); mp3.write(volume); mp3.write(0x7E); delay(10); while(mp3.available()) { if (0xA7==mp3.read()) return true; else return false; } } boolean SetPlayMode(uint8_t playmode) { if (((playmode==0x00)|(playmode==0x01)|(playmode==0x02)|(playmode==0x03))==false) { Serial.println("PlayMode Parameter Error! "); return false; } mp3.write(0x7E); mp3.write(0x03); mp3.write(0xA9); mp3.write(playmode); mp3.write(0x7E); delay(10); while(mp3.available()) { if (0xA9==mp3.read()) return true; else return false; } }
1. SetPlayMode(uint8_t playmode)
The Function is used to set the MP3 Play Mode.
uint8_t playmode: The parameter to change the play mode. Can be 0x00, 0x01, 0x02 or 0x03.
2. SetVolume(uint8_t volume)
The Function is used to set the MP3 Play Volume.
uint8_t volume: The parameter to change the play volume. The parameter range is 0x00 to 0x1F.
3. SetMusicPlay(uint8_t hbyte,uint8_t lbyte)
The Function is used to set the music index to play, the index is decided by the input sequence of the music
uint8_t hbyte: The high byte of the index;
uint8_t lbyte: The low byte of the index;
4. PauseOnOffCurrentMusic(void)
The Function is used to Pause on/off the current music.
- Now you can hear songs stored in your SD card. And in the playing mode, the D1 indicator is on. If in the pause mode, the indicator will blink. More experience is waiting for you!
There is another way to control MP3 play mode via serial tool.In this way, you need a UartSBee to connect MP3 to PC. The hardware installation as shown below:
After the connection is completed, open the serial tool to send commands. About the specific commands, please see the reference part!
More experience is waiting for you!
References¶
Common Command Descriptions:
Command Name | Command Format | Description |
---|---|---|
Pause | 7E 02 A3 7E | The music will stop when you send this command at the first time. After resending this command, it will continue. |
Stop | 7E 02 A4 7E | This command is able to trigger play the next song, or trigger play the first one if the player is playing the last one. |
Next | 7E 02 A5 7E | This command is able to trigger play the next song, or trigger play the first one if the player is playing the last one. |
Previous | 7E 02 A6 7E | This command can trigger play the previous song. Sending this command can trigger playback to the last song when you are enjoying the first one. |
Volume control | 7E 03 A7 1F 7E | There are 32 volume levels from 00 to 31. 00 is mute, and 31 for the maximum volume. |
Assigned play mode | 7E 03 A9 XX 7E | XX=00 means playing single without playback(default) |
XX=01 means the single repeated play mode | ||
XX=02 means that it is all tracks repeated playback mode. | ||
XX=03 stands for random pattern. |
Resources¶
- Grove - Serial MP3 Play Eagle File
- Grove - Serial MP3 Play Schematic in PDF format
- Demo code on github
- WT5001 Datasheet
Tech Support¶
Please do not hesitate to contact techsupport@seeed.cc if you have any technical issue. Or submit the issue into our forum.