Skip to main content

reTerminal DM Guide

Getting Started with reTerminal


Getting Started with reTerminal DMHardware and Interfaces Usage
This wiki will cover hardware specifications including LoRaWAN®, WiFi, BLE, RS485/RS232, CAN bus, 1000M Ethernet, USB, HDMI, in addition to other features. This wiki covers the installation of add-on hardware such as SSDs, cameras, PEO modules, assembly of WiFi/BLE antennas, LoRaWAN antennas, and more.

OS Installations


Raspbian OSSenseCraft Edge
This wiki will guide you through the installation process of Raspberry Pi OS and drivers. In this wiki, explore SenseCraft Edge OS, designed for reTerminal DM's 10.1" HMI device. It offers an intuitive interface with integrated functionalities for seamless device configuration and management.

Applications

Data Visualization

In this exciting section, get ready to discover how to whip up industrial-grade, interactive dashboards in few minutes!

Getting Start with FUXA - Web Based SCADA ToolreTerminal DM & Machinechat JEDI:Your Industrial IoT Powerhouse
In this section, we'll explore FUXA, a powerful web-based tool for quickly creating and deploying SCADA, HMI, Dashboard, or IIoT systems. With FUXA, you can easily design custom process visualizations, display real-time data, and control instruments in industrial settings. Machinechat JEDI simplifies IoT data management, enabling easy collection, visualization, monitoring, and response to real-time data. Paired with Seeed's reTerminal DM, crafting custom dashboards takes under 30 minutes.

Edge AI

Object detection with Edge Impulse and reTerminal DMTrain your own data set with Yolov5 and Deploy on reTerminal DM
In this wiki, we explore Object detection with Edge Impulse and reTerminal DM. Edge Impulse empowers developers to create and optimize embedded machine learning solutions using real-world data. Let's delve into the details. In this wiki, learn to train your own dataset with YOLOv5 and deploy it on your Raspberry Pi-based reTerminal DM.

Home Assistant

Frigate intergrating with reTerminal DM
Frigate is an open-source NVR designed for real-time AI object detection. All processing occurs locally on your hardware, ensuring your camera feeds stay within your home. This wiki guides you through the installation of the NVR and demonstrates object detection capabilities.

Cloud Solutions

AWS IoT Core Intergate With reTerminal DMAzure IoT Edge Intergate With reTerminal DM
AWS IoT Core securely connects and manages IoT devices, enabling communication with the cloud for smart applications. Our wiki will guide you through setting up the reTerminal DM device for seamless cloud communication. This Wiki describes how to connect reTerminal DM device running Debian 11 (ARM32v7) with Azure IoT Edge Runtime pre-installed and Device Management.

Industrial Edge

Node-red
reTerminal DM Getting Started with Node-RedreTerminal DM RS485 Port with Node-RED
In this wiki, we install Node-RED on reTerminal DM—an intuitive programming tool for connecting hardware devices, APIs, and online services through a browser-based editor, allowing easy flow creation and deployment with a single click. In this wiki, explore integrating Modbus devices into Node-RED workflows with the built-in Modbus node. Learn about the RS485 protocol, understand Modbus, and discover how to seamlessly integrate them with reTerminal DM.
reTerminal DM MQTT with Node-REDreTerminal DM CAN BUS with Node-RED
In this wiki, explore integrating MQTT into Node-RED, leveraging its support for this protocol to build powerful IoT applications. In this wiki, integrate a CAN bus module with Node-RED for efficient high-speed data exchange between ECUs, widely used in automotive, industrial automation, medical equipment, and aerospace applications

Ignition Edge
reTerminal DM Getting Started with Ignition EdgereTerminal DM Ignition Edge Panel Builder Hello World
By embedding Ignition Edge into field and OEM devices at the edge of the network, you can extend Ignition all the way to the edge of your network. Discover how to set up the reTerminal device with this guide. In this wiki, we will demonstrate how to create a basic page and display it at a fixed URL. We'll achieve this by creating a 'hello world' perspective project and viewing it on the gateway using a web browser.

N3uron
reTerminal DM Getting Started with N3uronConnect AWS IoT Core with N3uronIntegrating Historian Module for Visualizing on reTerminal DM
N3uron is your go-to Industrial Edge Platform for IIoT & DataOps, ensuring seamless integration between your plant floor and third-party applications, be it on-premises or in the cloud. In this tutorial, we'll kickstart your journey into the N3uron world. In this tutorial, we will delve into the intricacies of interfacing between the N3uron Edge IIoT platform and AWS IoT Core. With Neuron Historian, effortlessly store tag values collected locally or remotely via N3uron Links. It also provides a convenient Store & Forward feature for retaining data during communication loss. In this tutorial, you'll learn to create graphs and save your data as CSV files with ease.
                                                                                         

✨ Contributor Project

  • We have a task list for updating this page, which is categorized under our contributor project, as we are dedicated to enhancing the user experience and providing better support through the development of our wiki platform.
  • Your contribution to this page is essential to us! We really value your input and would greatly appreciate your assistance in generating ideas.

Tech Support & Product Discussion

Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.

Loading Comments...