Skip to main content

Deploy model to XIAO ESP32S3 on Sensecraft AI Platform

Getting Started

SenseCraft AI platform provide a very simple way to deploy AI model to edge device such as Jetson orin ,XIAO ESP32S3 Sense,etc. Enjoy seamless Edge AI model deployment now!

  1. Select or upload an AI model for XIAO ESP32S3

  2. Visit the AI model detail and click "Deploy Model" button

  1. Align the connector on the camera sensor expansion board with the B2B connector on the XIAO ESP32S3 Sense and press it to install camera sensor.

  1. Connect the XIAO ESP32S3 Sense to your computer via USB and Select USB JAG/serial debug unit to connect device.
note

Please use Chrome, Opera, or Edge to deploy AI models to XIAO ESP32S3 Sense and Grove Vision AI v2.

  1. Waiting for the model to be flashed. Once completed, the device will use the model for inference.

Tech Support

Need help with your SenseCAP Indicator? We're here to assist you!

Loading Comments...