Skip to main content

Grove - OLED Display 1.12 (SH1107) V3.0 - SPI/IIC -3.3V/5V

The Grove - OLED Display 1.12 V3.0 (SH1107) is a monochrome display with 128*128 resolution. Compared with LCDs, there are many advantages on OLED(Organic Light Emitting Diode) like self-emission, high contrast ratio, slim/thin outline, wide viewing angle and low power consumption. The display works on both 3.3V and 5V supply voltage. You can use either I2C or SPI interface to light up the display with your microcontroller to display words, images, and whatever you want.

pir

Feature​

  • 3.3V/5V power supply compatible
  • Changeable I2C address
  • SPI available
  • Low power consumption
  • monochrome 128×128 pixels
  • High contrast, high brightness
  • Wide operating temperature range: -40℃ ~ +85 ℃

Version​


Product VersionChangesReleased Date
Grove - OLED Display 1.12" V1.0InitialMar 2012
Grove - OLED Display 1.12" V2.1Change the driver IC from SSD1327 to SH1107G, upgrade the grayscale pixels from 96X96 to 128X128Nov 2015
Grove - OLED Display 1.12" V3.0Change the driver IC from SSD1107G to SH1107, upgrade the interface from I2C to I2C/SPIJuly 2021
tip

More details about Grove modules please refer to Grove System

Platforms Supported​


ArduinoRaspberry Pi

pir

pir

caution

The platforms mentioned above as supported is/are an indication of the module's software or theoritical compatibility. We only provide software library or code examples for Arduino platform in most cases. It is not possible to provide software library / demo code for all possible MCU platforms. Hence, users have to write their own software library.

Getting Started​

Hardware​

Here we will show you how this Grove - OLED Display works via a simple demo. First of all, you need to prepare the below stuffs:

Seeeduino V4Grove - OLED Display 1.12`` V3.0Base Shield

pir

pir

pir

Get ONE NowGet ONE NowGet ONE Now

This is an easy-to-use module, what you need to do is connect the module to I2C port of a Base Shield. There're 4 pins, defined as below.

pinFunctionNoteCable color
pin1SCLI2C ClockYELLOW
pin2SDAI2C DataWHITE
pin3VCCPower, 5V/3.3VRED
pin4GNDGroundBLACK

Hardware Overview (I2C)

Software (I2C)​

  • Step 1. Connect Grove - OLED Display 1.12'' V3.0. to I2C port of Base Shield via Grove cable.

  • Step 2. Open Arduino IDE and the Library Manager (Sketch > Include Library > manage Libraries) to install the library of u8g2.

  • Step 3. Enter "u8g2" into the search field and select latest version and Cclick "Install" button.
  • Step 4. Upload the demo code below in your Arduino IDE.
#include <Arduino.h>
#include <U8g2lib.h>
#include <SPI.h>
#include <Wire.h>

U8G2_SH1107_SEEED_128X128_1_SW_I2C u8g2(U8G2_R0, /* clock=*/ SCL, /* data=*/ SDA, /* reset=*/ U8X8_PIN_NONE);

void setup(void) {
u8g2.begin();
}

void loop(void) {
u8g2.firstPage();

do {
u8g2.setFont(u8g2_font_luBIS08_tf);
u8g2.drawStr(0,24,"Hello Seeed!");
} while ( u8g2.nextPage() );
}
success

There will be a "Hello Seeed!" displayed on the screen of Grove - OLED Display 1.12'' if everything goes well.

note

If there's no Base Shield with you, Seeeduino Vx Series with I2C interface do work as well.

Hardware Overview (SPI)

  • Step 1. Soldering male header and connect the wires.

  • Step 2. Please follow the YELLOW line to cut down the wire on the board and follow the WHITE line to solder the SPI pannels and the middle pannels one by one.

pir

caution

Please be careful to cut the wires one by one by following the YELLOW lines, otherwise you will damage all the display. We recommand you to cut the wires under magnifying glass.

Caution: This is the wrong method to cut wires!

pir

  • Step 3. Follow the picture to connect the display and Seeeduino with wires.
  • Step 4. Connect Seeeduino to a PC via a USB cable.

Software (SPI)​

  • Step 1. Open Arduino IDE and the Library Manager (Sketch > Include Library > manage Libraries) to install the library of u8g2.
  • Step 2. Enter "u8g2" into the search field and select latest version and Cclick "Install" button.
  • Step 3. Upload the demo code below in your Arduino IDE.
#include <Arduino.h>
#include <U8g2lib.h>
#include <SPI.h>
#include <Wire.h>

U8G2_SH1107_128X128_1_4W_HW_SPI u8g2(U8G2_R3, /* cs=*/ 10, /* dc=*/ 9, /* reset=*/ 8);

void setup(void) {
u8g2.begin();
}

void loop(void) {
u8g2.firstPage();

do {
u8g2.setFont(u8g2_font_luBIS08_tf);
u8g2.drawStr(0,24,"Hello Seeed!");
} while ( u8g2.nextPage() );
}
success

There will be a "Hello Seeed!" displayed on the screen of Grove - OLED Display 1.12'' if everything goes well.

Play on RaspberryPi​

Materials required

Raspberry piGrove Base Hat for Raspberry PiGrove - OLED Display 1.12" V3.0

pir

pir

pir

Get One NowGet ONE NowGet ONE Now

Get ready for RaspberryPi​

I2C Connection​

  • Step 1. Plug OLED Yellow&Blue Display 0.96" to I2C port of Grove - Base Hat.

  • Step 2. Plug Grove - Base Hat into RaspberryPi.

  • Step 3. Connect RaspberryPi to a PC via Serial or SSH.

SPI Connection​

  • Step 1. Follow the sheet to connect the wires on Grove - Base Hat.
Grove - OLED Display 1.12" V3.0 PinsRaspberry Pi GPIOBCM2835 Code
VCC3.3V3.3V
GNDGNDGND
SIMOSI10
SCLSCLK11
CSCE08
DCGPIO.625
RESGPIO.227
  • Step 2. Plug Grove - Base Hat into RaspberryPi.

  • Step 3. Connect RaspberryPi to a PC via Serial or SSH.

pir

Software​

  • Step 1. Enable I2C and SPI on RaspberryPi
sudo apt-get install -y i2c-tools
sudo raspi-config

Follow the pictures to enable I2C and SPI on your RaspberryPi.

pir

pir

pir

pir

pir

And then reboot your RaspberryPi

sudo reboot
  • Step 2. Install necessary libraries
sudo apt-get install wget gcc make unzip -y

Install WiringPi Library

If you use WiringPi, you need to update WiringPi to version 2.52. This library may not be updated. Other libraries are recommended

cd
sudo apt-get install wiringpi
wget https://project-downloads.drogon.net/wiringpi-latest.deb
sudo dpkg -i wiringpi-latest.deb
gpio -v

Install bcm2835

cd
wget http://www.airspayce.com/mikem/bcm2835/bcm2835-1.60.tar.gz
tar zxvf bcm2835-1.60.tar.gz
cd bcm2835-1.60/
sudo ./configure
sudo make && sudo make check && sudo make install

For more information and the newest libraries please refer to website:bcm2835

  • Step 3. Download the demo codes

1. For I2C

wget https://files.seeedstudio.com/wiki/Grove-OLED-Display-1.12-(SH1107)_V3.0/demo/RaspberryPiI2C.zip
mkdir I2C
unzip RaspberryPiI2C.zip ./I2C/
cd ./I2C/RaspberryPiI2C/c/
sudo chmod 777 test.sh
./test.sh

2. For SPI

wget https://files.seeedstudio.com/wiki/Grove-OLED-Display-1.12-(SH1107)_V3.0/demo/RaspberryPiSPI.zip
mkdir SPI
unzip RaspberryPiSPI.zip ./SPI/
cd ./SPI/RaspberryPiSPI/c/
sudo chmod 777 test.sh
./test.sh

If you want to have more demo, we also have a little video clip.

sudo chmod 777 badapple.sh
./badapple.sh

U8g2 Library Introduction​

U8g2 is a monochrome graphics library for embedded devices. U8g2 supports monochrome OLEDs and LCDs, which include our chip SSD1327/SH1107G.

The Arduino library U8g2 can be installed from the library manager of the Arduino IDE. U8g2 also includes U8x8 library:

U8g2

  • Includes all graphics procedures (line/box/circle draw).
  • Supports many fonts. (Almost) no restriction on the font height.
  • Requires some memory in the microcontroller to render the display.

U8x8

  • Text output only (character) device.
  • Only fonts allowed with fit into a 8x8 pixel grid.
  • Writes directly to the display. No buffer in the microcontroller required.

Here provides the U8g2 Library wiki as well as the U8g2 API Reference page.

Schematic Online Viewer​

Resources​


Tech Support & Product Discussion​

Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.

Loading Comments...