How to Use SenseCAP AI on SenseCAP Portal and SenseCAP Mate APP
Overview
SenseCAP AI is the AI-powered solution that helps you make the most of your sensor data and unlock the full potential of your sensor data. By connecting your SenseCAP sensors to the SenseCAP platform, you can easily collect and analyze data on environmental factors such as temperature, humidity, light, and air quality. Meanwhile, our powerful AI algorithms then use this data to provide you with actionable insights and recommendations that can help you optimize your operations, reduce costs, and improve efficiency.
Whether you're looking to monitor air quality, optimize crop growth, or improve efficiency, SenseCAP AI has the tools you need to succeed. SenseCAP AI is currently released on SenseCAP Portal and SenseCAP Mate App, where users can use it at any time. With our easy-to-use platform and App, you can quickly connect your sensors and start receiving valuable insights in just minutes.
Don't miss out on the benefits of AI-powered sensor data analysis. Try SenseCAP AI today!

Measurements
SenseCAP AI currently analyzes the following measurements and device types, and users can select devices that include the following measurements.
SenseCAP Mate App
1 Download and login SenseCAP Mate App
2 Visit Device page and click + icon to bind your SenseCAP sensor by scaning the device QR code
3 Make sure your sensor sends data to the SenseCAP platform, the SenseCAP AI service needs to use the sensor's data
4 On Device page click SenseCAP AI to start AI-powered sensor data analysis

5 Enter the crop or animal you are raising and the location
6 Select the sensor data time
- Month: sensor data in the last month
- 6 Months: sensor data in the last 6 months
- Year: sensor data in the last year
7 Select measurement(up to 5 ): click + icon
- Select device and then select measurement

8 Send the info to SenseCAP AI and then SenseCAP AI will response suggestions
Note:AI answers are provided for reference only. Please use them with caution as SenseCAP cannot be held responsible for any consequences resulting from the use of AI services.

SenseCAP Portal
1 Login SenseCAP Portal(Global)
2 Bind your SenseCAP sensor by inputing sensor's SN and code

3 Make sure your sensor sends data to the SenseCAP platform, the SenseCAP AI service needs to use the sensor's data
4 Visit SenseCAP AI to start AI-powered sensor data analysis
5 Enter the crop or animal you are raising and the location
6 Select the sensor data time
- Month: sensor data in the last month
- 6 Months: sensor data in the last 6 months
- Year: sensor data in the last year
7 Select measurement(up to 5 ): click + icon
- Select device and then select measurement

8 Send the info to SenseCAP AI and then SenseCAP AI will response suggestions
Note:AI answers are provided for reference only. Please use them with caution as SenseCAP cannot be held responsible for any consequences resulting from the use of AI services.