4G Raspberry Pi HAT - MBIM Mode Setup on Windows
Introduction
The Quectel 4G Raspberry Pi HAT supports internet connectivity on Windows by utilizing MBIM (Mobile Broadband Interface Model) mode. This mode enables Windows to recognize the 4G module as a native cellular modem, facilitating a stable and driver-supported network connection.
This guide will walk you through the necessary steps to configure your Quectel module in MBIM mode and connect it to the internet on Windows 10/11 systems.
Prerequisites
Hardware Requirements
| Raspberry Pi 5 | Raspberry Pi 4G LTE CAT4 HAT |
|---|---|
![]() | ![]() |
Software Prerequisites
Before proceeding, ensure that:
- Any previously installed Quectel NDIS or other drivers are uninstalled.
- The correct MBIM driver is installed using the links provided below.
MBIM Driver Download
Once installed, you can verify driver installation by navigating to Computer Management → Device Manager. A successful installation will show devices under "Network Adapters" and "Ports (COM & LPT)" similar to the image below:
Configure MBIM Mode
To switch the module to MBIM mode, you will need the QCOM Tool.
-
Download and open the QCOM Tool.
-
Connect your 4G HAT to your Windows PC via USB and power it on.
-
In QCOM, send the following AT command to check the current USB mode:
AT+QCFG="usbnet"?- If it returns anything other than
"usbnet",2, skip this.
- If it returns anything other than
-
To switch to MBIM mode, send:
AT+QCFG="usbnet",2 -
Then reboot
AT+CFUN=1,1
Sometimes you may experience the AT port not responding. In such cases, use the DM port instead.
Connect to Network
Once configured in MBIM mode:
- Windows should detect a Cellular Network Interface.
- You can now manage and connect to networks directly from the Windows Network & Internet Settings.
Verify Network Configuration
To verify if your PC has acquired a network connection via MBIM:
-
Open Command Prompt.
-
Run:
ipconfigYou should see an interface with an IP address under "Mobile Broadband Connection" or "Cellular".
Tech Support & Product Discussion
Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.