Skip to main content

Get Started with T1000-E Tracker

note

When the device is in the states below, please don't manually reboot or turn off it. Or else the device can be dead.

  1. Not finishing the message transmission process
  2. Being configured

Video Tutorial

Part 1: Unboxing Setup

Part 2: Status Indicators

Part 3: Flash New Firmware

note

Before flashing the firmware, please ensure you bought the T1000-E for Meshtastic. Please don't flash the firmware to other tracker model that doen't support Meshtastic. Please don't use NRF-OTA to update the firmware, it may cause the device to be completely dead.

Part 4: Troubleshooting Instruction

Get Started

Download Meshtastic App:

Power on the device

Press once to power on the device, there will be a rising melody, and the LED light will stay on for about 1s.

tip

If the device doesn't respond when you press the button, please charge it first. Do not use the fast-charging charger.

Connect via App

  • Select the target device on the Bluetooth panel.

pir

  • Enter the code(default code is 123456) and then click OK to connect the device.

pir

Connect via Website

If you want to text messages and communicate with other nodes in the website, you can connect the device to the Meshtastic Website now.

Step 1: Open the Website

Click here to go to the webstite.

pir

Step 2: Add the new device

Click "+ New Connection".

pir

There are two ways to connect. You can choose your preferred method.

Method 1: Via Bluetooth

Choose bluetooth method. Choose the device ID in the pop-up window.

pir

Method 2: Via Serial

Choose serial method. Open the device manager to see which port the device is connected to. Choose that port in the pop-up window.

pir

Your device will be shown in the list. Click to connect. If the connection succeed, you can see the device status directly on the website.

pir

Configuration

Configure the LoRa

In order to start communicating over the mesh, you must set your region. This setting controls which frequency range your device uses and should be set according to your regional location.

pir

Region List

Region CodeDescriptionFrequency Range (MHz)Duty Cycle (%)Power Limit (dBm)
UNSETUnsetN/AN/AN/A
USUnited States902.0 - 928.010030
EU_868European Union 868MHz869.4 - 869.651027

Refer to LoRa Region by Country for a more comprehensive list.

info

EU_868 has to adhere to an hourly duty cycle limitation of 10%, calculated every minute on a rolling 1-hour basis. Your device will stop transmitting if you reach it, until it is allowed again.

Now that you have set the LoRa region on your device, you can continue with configuring any LoRa Configs to suit your needs.

(Optional) Configure Sensor

SensorDescription
Temperature
LightNot supported by the App currently
AccelerometerTo be continued

Temperature Sensor Config

Navigate to Settings -> Telemetry(Sensors) -> Enable sensors.

pir

Buzzer and LED Config

TypeOutput PIN
BuzzerPWM buzzer25
LED-24

Navigate to Settings -> External Notification -> Enable GPIO -> Set Output Pin GPIO.

pir

Check External Notification Config for more details.

tip

After you update the device configuration, the device will restart, which may take some time.

(Optional) Configure Ringtone

Navigate to Settings -> Ringtone Config, then enter the RTTTL ringtone string you want to use for external notifications.

pir

You can paste one of the following RTTTL examples directly:

The Legend of Zelda: Item Get

24:d=16,o=5,b=120:g,c6,d6,2g6

Super Mario Theme (Short)

24:d=4,o=5,b=100:16e6,16e6,32p,8e6,16c6,8e6,8g6,8p,8g

Mario Coin

24:d=8,o=6,b=200:b,e7

Mario Power-Up

powerup:d=16,o=5,b=200:g,a,b,c6,d6,e6,f#6,g6,a6,b6,2c7

Nokia Ringtone

24:d=4,o=5,b=180:8e6,8d6,f#,g#,8c#6,8b,d,e,8b,8a,c#,e,2a

Morse Code CQ

24:d=16,o=6,b=120:8c,p,c,p,8c,p,c,4p,8c,p,8c,p,c,p,8c,8p

Demo Video

(Optional) Configure GPS

Please set GPS enabled. You can adjust the update inerval and broadcast interval to obtain a more up-to-date location information.

pir

For IOS, please turn on the Accurate Location. Otherwise, the positioning may deviate.

pir

(Optional) Configure Buzzer

The buzzer is enabled by default. If you want to disable the buzzer, set Alert Message buzzer, Alert bell buzzer and Use PWM bizzer as the following screenshot.

pir

Flash Firmware

Check the Firmware Version

Navigate to Settings -> Firmware Updates, check the current firmware version.

pir

⚠️DO NOT FLASH THE FOLLOWING FIRMWARE

danger

DO NOT FLASH OTHER FIRMWARE OTHER THAN T1000-E FIRMWARE, THIS MAY CAUSE THE DEVICE TO FREEZE.

The following firmware will brick your device:

  • nrf52_promicro_diy_tcxo
  • nrf52_promicro_diy_xtal
  • Dongle_nRF52840-pca10059-v1
  • feather_diy
  • TWC_mesh_v4
  • wio-sdk-wm1110
  • wio-tracker-wm1110
  • xiao_ble

Flash the Application Firmware

note

Before flashing the firmware, please ensure you bought the T1000-E for Meshtastic. Please don't flash the firmware to other tracker model that doen't support Meshtastic. Please don't use NRF-OTA to update the firmware, it may cause the device to be completely dead.

Step 1: Enter DFU mode

Visit Meshtastic Web Flasher.

Connect the device to your PC, select the device to Seeed Card Tracker T1000-E and choose the latest firmware, then click Flash.

pir

Click Enter DFU Mode, there will be a serial port named T1000-E xxx display, click and connect it, the green LED will be solid, and there should be a driver named T1000-E display.

pir

pir

Step 2: Flash Erase

note

Before flashing the firmware, please flash the erased firmware first!

Click the trash symbol.

pir

Download the erase firmware and copy to the driver.

pir

This process may take some time, wait for the drive to disappear, then open a serial monitor to complete the erase process.

Step 3: Flash Firmware

Select the latest firmware, and download the UF2 file.

pir

Copy UF2 file to the DFU drive. Firmware should be flashed after the file is downloaded and the device reboots.

FAQ

How to check the device name

Visit Meshtastic Web Flasher.

Click Open Serial Monitor, connect the device to your PC, check the serial log, keyword using nodenum.

pir

pir

How to reboot the device

Press and hold the button, then connect the charging cable.

Troubleshooting

Device never turns on

  • Charge the device for 1~2 hours

  • Unplug the USB cable, then hold the button down and plug the usb cable back in while continuing to hold the button for 5 seconds.

  • Change the charging cable

  • Sometimes it looks like turning off, but in fact it is because the LED and the buzzer have not been activated. Check the following parameters:

pir

  • If still no luck, press and hold the device button, then connect the charging cable, see whether or not the a disk pop out in your PC. If so, click here to re-install the bootloader

Device stuck in boot loop

Description:

The device will restart repeatedly, and the serial port connects and disconnects repeatedly.

Solution:

  • Step 1: Try to enter DFU mode manually: press and hold the device button, then quickly connect the charging cable twice, the green LED will be solid on.
note

To successfully enter the DFU mode, you need to perform this operation quickly. You may need to try multiple times.

pir

Device bricked

Description

The device not responding, no LED, can not pair with your App.

1) Device can still enter the DFU mode, then try to flash the bootloader.

Flash the Bootloader

note

When you are flashing the bootloader, please make sure the cable connection is stable and DO NOT disconnect it during the flash process.

Step1: Adafruit-nrfutil Installation

For window user, press "Win" key and "r" key, then enter "cmd" in the pop-oyt window, click "Enter". This can open the command line.

For MAC user, press "Command" key and "Space" key, so that you can open Spotlight. Then enter "termial", click "Return". This can open the command line.

Prerequisites

Check in your command line that whether or not the python and pip are installed successfully.

python --version
python -m pip --version

Then "Python xxx" and "pip xxx" should appear. If it does not, please try install python again.

This is recommended method, to install latest version:

pip3 install --user adafruit-nrfutil

Check the installation path:

python -m pip show adafruit-nrfutil

This is the installation location:

pir

For window user, you may need to add the path manually. Copy the installation location showed in the last step. Then add it as followed:

pir

Step2: Check your port number

Connect your device to your PC, and check the port number.

For Window User, open your device manager, and go to "port", the port number newly pop out after the device connection is the device port number.

For Mac user, for example:

pir

For Window user, for example:

pir

Step3: Flash the bootloader

In the terminal or command prompt, navigate to the directory where you downloaded the bootloader zip package and execute the following command, replacing the correct port for your device:

  • For Windows:
adafruit-nrfutil --verbose dfu serial --package t1000_e_bootloader-0.9.1-5-g488711a_s140_7.3.0.zip -p COMxx -b 115200 --singlebank --touch 1200

Please change COMXX to your com number. For example, if your device is on com6, change the command to be:

adafruit-nrfutil --verbose dfu serial --package t1000_e_bootloader-0.9.1-5-g488711a_s140_7.3.0.zip -p **COM6** -b 115200 --singlebank --touch 1200

Some of the device will change their port number after you enter this command. So if the installation fail, check the port number again.

  • For others:
adafruit-nrfutil --verbose dfu serial --package t1000_e_bootloader-0.9.1-5-g488711a_s140_7.3.0.zip -p /dev/tty.SLAB_USBtoUART -b 115200 --singlebank --touch 1200

pir

When you have completed the above steps, then you can follow this step to flash the application firmware.

2) Device can not enter DFU mode, but the serial port can be detected.

  • Open a serial port tool

  • Set the baud rate to 1200.

  • Connect the device. The light will flash briefly when you connect it. Keep trying this until the light stays on, means the device can back to DFU mode, then flash bootloader -> Erase flash -> flash the firmware.

3) Device can not enter DFU mode and no serial port display

  • press and hold the device button, then connect the charging cabl. After a disk pop out in your PC, you may see the serial port.

  • If still no luck, please disconnect the charging cable and leave the device for a few days until the battery is completely drained, then connect the charging cable and try to pair it again.

4) If none of the above steps work, please contact the tech support: [email protected]

Firmware flashing failed

  • No data received on serial port

pir

Check if the device is in the DFU mode, the green light will be solid when the device is in DFU mode.

  • Can't open serial port

pir

Check if the port is correct, or try another port.

Device automatically turn off

Description

  • After the device turning on, it will turn off or reboot automatically after a while.
  • The serial port log ran for a while and then stopped.

This is possibly caused by manually and forcely rebooting or turning off the device when the device is in the following states:not finishing the messages transmission process, being configured......

Troubleshoot

Click here to perform a flash-erase.

Factory Reset

If you want to restore to the default settings, you can do the factory reset. There are two methods for you to do the factory reset.

  • Click here to flash erase the device. And then re-flash the latest firmware.

  • Click the Factory Reset Button on the App. The device will reboot with the factory configuration automatically.

    pir

NodeDB Reset

NodeDB is the local database that stores information about nodes discovered in the current Mesh network, including:

  • Node ID
  • User Name
  • Location Information
  • Signal Information (SNR)
  • Last Seen Time

When to reset

Reset NodeDB when:

  • The node list contains outdated, duplicate, or invalid entries.
  • You move to a different Mesh environment and want to rediscover nearby nodes.
  • Node information in the app appears incorrect or incomplete.
danger

Resetting NodeDB only clears the node database stored on the device. It does not perform a factory reset and does not remove the device's basic configuration.

Reset from the App

  1. Open the app and connect to the target device.
  2. Go to Settings.
  3. Tap Device.
  4. Scroll to the bottom of the Device Config page and find Reset NodeDB.
  5. Tap it and confirm the action.

App Path

Settings > Device > Reset NodeDB

Example Screens

Step 1: Open Device from the Settings page.

Device entry in Settings

Step 2: Tap Reset NodeDB on the Device Config page.

Reset NodeDB button in Device Config

tip

Please note the difference between the following options:

  • Reset NodeDB: Only clears the node database.
  • Factory Reset: Restores the device to factory settings and removes more configuration data.

What happens after reset

After Reset NodeDB is executed, the device clears the currently stored node list. As the device continues running, it will rediscover and record nearby nodes again.

You may observe the following:

  • The node list may temporarily become empty or smaller.
  • Nodes will gradually reappear as the device continues operating.
  • Previously stored historical node records will no longer be available.

Notes

  • Before resetting, make sure the issue is actually related to an abnormal node list.
  • If the problem is only a delay in node display, wait for a while first to see whether it recovers automatically.
  • If the issue remains after resetting NodeDB, continue troubleshooting the device configuration or other possible causes.
  • Use Factory Reset carefully to avoid accidentally removing device configuration.

Signal Quality

  • SNR reflects the quality of the communication link. Normal device usually operates above -7 dB. Device with a SNR lower than -10 dB indicates poor performance.

  • RSSI is determined jointly by the device and its surrounding environment. Normal device usually operates above -110 dBm. Device with an RSSI lower than -115 dBm is considered to have poor performance.

    To achieve the best signal effect, please use the device in an open, unobstructed area with minimal interference for use.

Pogo Pin Definition

pir

Resources

Tech Support & Product Discussion

Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.

Loading Comments...