Skip to main content

XIAO ESP32S3(Sense) With FreeRTOS

This wiki covers FreeRTOS support for the Seeed Studio XIAO ESP32S3. With the assistance of this guide you will be able to utilize the feature set available to the board.

What is FreeRTOS

pir

FreeRTOS is a collection of C libraries comprised of a real-time kernel and a set of modular libraries that implement complementary functionality. The FreeRTOS kernel is a real-time kernel (or real-time scheduler) that enables applications built on FreeRTOS to meet their hard real-time requirements. It enables applications to be organized as a collection of independent threads of execution.

Reference : Mastering the FreeRTOS Real Time Kernel

FreeRTOS ports

FreeRTOS is an open source RTOS (real-time operating system) kernel that is integrated into ESP-IDF as a component. Thus, all ESP-IDF applications and many ESP-IDF components are written based on FreeRTOS. The FreeRTOS kernel is ported to all architectures (i.e., Xtensa and RISC-V) available of ESP chips.

We will be using the ESP IDF port of the FreeRTOS.

Hardware Preparation

I am using Seed Studio XIAO ESP32S3 Sense and the onboard camera, microphone and sd-card reader along with the Wifi functionality of the ESP32S3.

Seeed Studio XIAO ESP32S3(Sense)

Additional Components

Software Preparation

I am using Visual Studio Code (Windows) with ESP-IDF.

  1. VSCode install
  2. ESP-IDF installation guide
  3. Git Repository

Getting Started

Setting up ESP-IDF

After setting up the Visual Studio Extension, open the terminal and paste the following command to access the ESP-IDF Command Line Tools from the normal terminal environment(outside of VScode).

note

The normal installation of ESP-IDF extension of VS-Code will take care of 90% of use cases do the following steps only if you need ESP Command line tools outside of the environment.

PowerShell (Windows)

.$HOME\esp\v5.3\esp-idf\export.ps1
info

".$HOME\esp\v5.3\esp-idf" may differ from user to user.This the default installation path.
Replace it wil the installation path on your device.

tip

To avoid repeated setup boot up PowerShell in administrator mode and type the following command

notepad $PSHOME\Profile.ps1

A Notepad instance will open up. Paste the export shell command in the note-pad and save it. open an instance of powershell and it should have close to the following output.

Done! You can now compile ESP-IDF projects.

If everything is done properly, the following command :

idf.py

should show the following output :

Usage: idf.py [OPTIONS] COMMAND1 [ARGS]... [COMMAND2 [ARGS]...]...

ESP-IDF CLI build management tool. For commands that are not known to idf.py an attempt to execute it as a build
system target will be made. Selected target: None

Board Configuration for XIAO ESP32S3

After setting up ESP-IDF, you need to configure your project specifically for the XIAO ESP32S3 board to take advantage of its hardware features including 8MB Flash and 8MB Octal PSRAM.

Set Target Device

In your ESP-IDF project directory, set the target to ESP32-S3:

idf.py set-target esp32s3

Enable Full Build Options

In your project's root CMakeLists.txt, ensure MINIMAL_BUILD is set to OFF:

idf_build_set_property(MINIMAL_BUILD OFF)

This enables all configuration options in menuconfig.

Configure Flash and PSRAM

Open the configuration menu:

idf.py menuconfig

Flash Size Configuration:

  1. Navigate to: Serial flasher config → Flash size
  2. Set to: 8 MB

PSRAM Configuration:

  1. Navigate to: Component config → ESP PSRAM
  2. Enable: Support for external, SPI-connected RAM
  3. Set SPI RAM mode to: Octal Mode PSRAM
  4. Set SPI RAM clock to: 80MHz
info

The XIAO ESP32S3 uses Octal PSRAM, not Quad mode. Selecting the correct mode is essential for the 8MB PSRAM to function properly.

Update Main Component Dependencies

In /main/CMakeLists.txt, ensure PSRAM and SPI flash components are included:

idf_component_register(
SRCS "main.c"
INCLUDE_DIRS "."
PRIV_REQUIRES esp_psram spi_flash
)

Create Board Pin Configuration Component

Create a reusable component for XIAO pin definitions to make your code more readable and portable:

mkdir -p ./components/board_config/include/

Create ./components/board_config/include/xiao_pins.h:

// xiao_pins.h
#pragma once

#ifdef __cplusplus
extern "C" {
#endif

// Analog / Digital Pins
#define XIAO_D0 1
#define XIAO_D1 2
#define XIAO_D2 3
#define XIAO_D3 4
#define XIAO_D4 5
#define XIAO_D5 6
#define XIAO_D6 43
#define XIAO_D7 44
#define XIAO_D8 7
#define XIAO_D9 8
#define XIAO_D10 9

// Onboard User LED (Active Low)
#define XIAO_LED 21

// I2C Pins (Default)
#define XIAO_SDA 5 // Same as D4
#define XIAO_SCL 6 // Same as D5

// SPI Pins (Default)
#define XIAO_MISO 9 // Same as D10
#define XIAO_MOSI 10
#define XIAO_SCK 8 // Same as D9
#define XIAO_SS 7 // Same as D8

#ifdef __cplusplus
}
#endif

Create ./components/board_config/CMakeLists.txt:

idf_component_register(INCLUDE_DIRS "include")
tip

These pin definitions match the silkscreen labels on the XIAO ESP32S3 board, making your code more readable. For example, use XIAO_LED instead of hard-coding GPIO 21.

Use Pin Definitions in Your Code

In your main application or any component, include the header:

#include "xiao_pins.h"

void app_main(void) {
// Example: Configure LED pin
gpio_set_direction(XIAO_LED, GPIO_MODE_OUTPUT);
gpio_set_level(XIAO_LED, 0); // Turn on (active low)
}

Pin Mapping Reference

Xiao ESP32S3 Pinout reference picture

LabelGPIOAlt Function
D01ADC1_CH0
D12ADC1_CH1
D23ADC1_CH2
D34ADC1_CH3
D45ADC1_CH4, SDA
D56ADC1_CH5, SCL
D643TX
D744RX
D87ADC1_CH6, SS
D98ADC1_CH7, SCK
D109ADC1_CH8, MISO
note
  • GPIO 19 and 20 are used for USB D-/D+ and should not be reconfigured
  • The onboard LED on GPIO 21 is active LOW (set to 0 to turn on)
  • All pins D0-D10 support analog input via ADC1

Building and Flashing

Build your project:

idf.py build

Flash to the XIAO ESP32-S3:

idf.py -p /dev/ttyACM0 flash monitor

Replace /dev/ttyACM0 with your actual serial port (on Windows, typically COM3, COM4, etc.).

Troubleshooting Board Configuration

PSRAM Not Detected:

  • Verify Octal mode is selected (not Quad)
  • Check that flash size is set to 8MB
  • Ensure ESP-IDF version is 4.4 or later

Upload Fails:

  • Press and hold the BOOT button while connecting USB
  • Try reducing upload speed: idf.py -p PORT -b 115200 flash

Pin Conflicts:

  • Avoid using GPIO pins 19 and 20 (USB D- and D+)
  • XIAO_LED (GPIO 21) is shared with the onboard LED

What are Task?

Tasks are small functions/ jobs that the the processor is requested to perform with a set of settings. Tasks can range from small functions to infinite looping functions.
Tasks are the fundamental units of execution in an ESP-IDF application. They are essentially functions that run concurrently with other tasks. This allows for efficient multitasking and responsiveness.

What are task properties?

Due to the vastness of this topic, i will be only covering a few of the properties we will be using for this guide.

  • TaskFunction: This is the function that contains the actual logic of the task. It's the entry point for the task's execution.
  • StackSize: This specifies the amount of memory allocated for the task's stack. The stack is used to store local variables, function return addresses, and temporary data.
  • TaskPriority: This determines the relative importance of the task compared to other tasks. Higher-priority tasks have a greater chance of being executed before lower-priority ones.
  • TaskParameters: These are optional arguments that can be passed to the task function when it's created. They can be used to provide additional context or configuration to the task.
  • CoreAffinity: This specifies which CPU core the task should be assigned to. In systems with multiple cores, this can be used to optimize performance or balance the workload.

Creating a task

To create a task in FreeRTOS, the xTaskCreate function is used. This function takes several parameters, including the task function, task name, stack size, parameters, priority, and a handle to the created task.

TaskHandle_t task;
xTaskCreate(
taskFunction, /* Function that implements the task. */
"taskName", /* Text name for the task. */
configMINIMAL_STACK_SIZE, /* Stack size in words, or bytes. */
NULL, /* Parameter passed into the task. */
tskIDLE_PRIORITY, /* Priority at which the task is created. */
&task /* Used to pass out the created task's handle. */
);

Creating a task pinned to a core

To create a task and pin it to a specific core (only if the chip in use is dual core), the xTaskCreatePinnedToCore function is used. This function is similar to xTaskCreate but includes an additional parameter for specifying the core.

TaskHandle_t task;
xTaskCreatePinnedToCore(
taskFunction, /* Function that implements the task. */
"taskName", /* Text name for the task. */
configMINIMAL_STACK_SIZE, /* Stack size in words, or bytes. */
NULL, /* Parameter passed into the task. */
tskIDLE_PRIORITY, /* Priority at which the task is created. */
&task, /* Used to pass out the created task's handle. */
0); /* Core ID */

Task function call

The task function is the actual code that will be executed by the task.

void taskFunction(void * pvParameters) {
/*
Function definition goes here
*/
}

Visualization of tasks

I am creating four simple task to visualize how the FreeRTOS works.

pir

Visual Representation

CPU0
-----
taskFunction1 (1000ms delay)

CPU1
-----
taskFunction2 (500ms delay)
taskFunction3 (500ms delay)
taskFunction4 (500ms delay)

Code

#include <stdio.h>
#include "freertos/FreeRTOS.h"
#include "freertos/task.h"
#include "sdkconfig.h"
#include "esp_log.h"

TaskHandle_t task1,task2,task3,task4;

void taskFunction1(void * pvParameters) {
while (true) {
ESP_LOGI("Task1", "Hello from task 1");
vTaskDelay(pdMS_TO_TICKS(1000)); // Add a delay to avoid overwhelming the output
}
}

void taskFunction2(void * pvParameters) {
while (true) {
ESP_LOGI("Task2", "Hello from task 2");
vTaskDelay(pdMS_TO_TICKS(500)); // Add a delay to avoid overwhelming the output
}
}

void taskFunction3(void * pvParameters) {
while (true) {
ESP_LOGI("Task3", "Hello from task 3");
vTaskDelay(pdMS_TO_TICKS(500)); // Add a delay to avoid overwhelming the output
}
}

void taskFunction4(void * pvParameters) {
while (true) {
ESP_LOGI("Task4", "Hello from task 4");
vTaskDelay(pdMS_TO_TICKS(500)); // Add a delay to avoid overwhelming the output
}
}

void app_main(void) {
xTaskCreatePinnedToCore(
taskFunction1, /* Function that implements the task. */
"task_1", /* Text name for the task. */
configMINIMAL_STACK_SIZE, /* Stack size in words, not bytes. */
NULL, /* Parameter passed into the task. */
tskIDLE_PRIORITY, /* Priority at which the task is created. */
&task1, /* Used to pass out the created task's handle. */
0); /* Core ID */

xTaskCreatePinnedToCore(
taskFunction2, /* Function that implements the task. */
"task_2", /* Text name for the task. */
configMINIMAL_STACK_SIZE, /* Stack size in words, not bytes. */
NULL, /* Parameter passed into the task. */
tskIDLE_PRIORITY, /* Priority at which the task is created. */
&task2, /* Used to pass out the created task's handle. */
1); /* Core ID */

xTaskCreatePinnedToCore(
taskFunction3, /* Function that implements the task. */
"task_3", /* Text name for the task. */
configMINIMAL_STACK_SIZE, /* Stack size in words, not bytes. */
NULL, /* Parameter passed into the task. */
tskIDLE_PRIORITY, /* Priority at which the task is created. */
&task3, /* Used to pass out the created task's handle. */
1); /* Core ID */

xTaskCreatePinnedToCore(
taskFunction4, /* Function that implements the task. */
"task_4", /* Text name for the task. */
configMINIMAL_STACK_SIZE, /* Stack size in words, not bytes. */
NULL, /* Parameter passed into the task. */
tskIDLE_PRIORITY, /* Priority at which the task is created. */
&task4, /* Used to pass out the created task's handle. */
1); /* Core ID */
}
tip

configMINIMAL_STACK_SIZE can be changed in sdkconfig.

  1. Four Tasks: The code defines four tasks: taskFunction1, taskFunction2, taskFunction3, and taskFunction4.
  2. Task Priorities: All tasks are created with the tskIDLE_PRIORITY. This means they have the same priority.
  3. Task Pinning: taskFunction1 is pinned to CPU0, while the other three tasks are pinned to CPU1.
  4. Task Delays: taskFunction1 has a delay of 1000ms, while the other three have a delay of 500ms.

Creating the CPU0 and CPU1 Task Schedule

I have create a basic task schedule for CPU0 and CPU1.

CPU0 Task Schedule

Task: taskFunction1
Priority: Idle (lowest)
Delay: 1000ms
Core: 0

CPU1 Task Schedule

Tasks: taskFunction2, taskFunction3, taskFunction4
Priorities: All Idle (same priority)
Delays: 500ms for all tasks
Core: 1
info

This is a simplified schedule. Actual task scheduling in a real-time system would involve more complex factors like task priorities, deadlines, and resource constraints.

Output
I (11412) Task1: Hello from task 1
I (11522) Task3: Hello from task 3
I (11522) Task2: Hello from task 2
I (11532) Task4: Hello from task 4
I (12032) Task3: Hello from task 3
I (12032) Task2: Hello from task 2
I (12042) Task4: Hello from task 4
I (12422) Task1: Hello from task 1
I (12542) Task3: Hello from task 3
I (12542) Task2: Hello from task 2
I (12552) Task4: Hello from task 4
I (13052) Task3: Hello from task 3
I (13052) Task2: Hello from task 2
I (13062) Task4: Hello from task 4
I (13432) Task1: Hello from task 1
I (13562) Task3: Hello from task 3
I (13562) Task2: Hello from task 2
I (13572) Task4: Hello from task 4
I (14072) Task3: Hello from task 3
I (14072) Task2: Hello from task 2
I (14082) Task4: Hello from task 4

Sensor polling using FreeRTOS

For this I am using an analog sensor Air Quality Sensor v1.3 along with ESP_IDF_v5.3.

Hardware Setup

Attach the Xiao-S3 to the Grove - Expansion Board and connect the Air Quality Sensor v1.3 to the analog connector.

pir

Software Setup

After pulling the git repository, open the folder in VSCode. Go to View->Command Palette->ESP-IDF: Add vscode Configuration Folder. From the bottom panel select the correct COM port, chip (ESP-S3) and build,flash and monitor.

Code Overview

This code is designed to collect air quality data from a sensor, process the raw data to determine the air quality level, and periodically print the results to the console.

Key Components

  • Sensor Initialization:
air_quality_sensor_t air_quality_sensor;

void sensor_setup()
{
air_quality_sensor._io_num = ADC_CHANNEL_0;
air_quality_sensor._adc_num = ADC_UNIT_1;
printf("Starting Air Quality Sensor...\n");
if(!initialize_air_quality_sensor(&air_quality_sensor))
{
printf("Sensor ready.\n");
}
else{
printf("Sensor ERROR!\n");
}
}
  • sensor_setup() function configures the sensor's I/O pins and ADC unit.

  • It attempts to initialize the sensor using initialize_air_quality_sensor().

  • If initialization is successful, the sensor is ready for data collection.

  • Data Collection Task:

void poll_read_air_quality_sensor(void *pvParameters)
{
for (;;)
{
air_quality_sensor_slope(&air_quality_sensor);
vTaskDelay(500 / portTICK_PERIOD_MS);
}
}
  • poll_read_air_quality_sensor() task is created to continuously read raw data from the sensor.

  • It calls air_quality_sensor_slope() to process the raw data and calculate the slope, which is an indicator of air quality.

  • The task delays for 500 milliseconds before reading the next data point.

  • Data Printing Task:


void print_read_air_quality_sensor(void *pvParameters)
{
for (;;)
{
char buf[40];
air_quality_error_to_message(air_quality_sensor._air_quality,buf);
printf("Time : %lu\tSlope : %d\tRaw Value : %d\n%s\n", (uint32_t)esp_timer_get_time() / 1000, air_quality_sensor._air_quality, air_quality_sensor._sensor_raw_value,buf);
vTaskDelay(1000 / portTICK_PERIOD_MS);
}
}
  • print_read_air_quality_sensor() task is created to periodically print the collected data and calculated air quality.
  • It retrieves the current time, slope, raw value, and air quality message using air_quality_error_to_message().
  • The task prints the data to the console in a formatted manner.
  • The task delays for 1000 milliseconds before printing the next data point.

void app_main(void)
{
sensor_setup();
xTaskCreatePinnedToCore(
poll_read_air_quality_sensor, /* Function that implements the task. */
"poll_read_air_quality_sensor", /* Text name for the task. */
configMINIMAL_STACK_SIZE * 2, /* Stack size in words, not bytes. */
NULL, /* Parameter passed into the task. */
tskIDLE_PRIORITY, /* Priority at which the task is created. */
NULL, /* Used to pass out the created task's handle. */
0); /* Core ID */

xTaskCreatePinnedToCore(
print_read_air_quality_sensor, /* Function that implements the task. */
"print_read_air_quality_sensor", /* Text name for the task. */
configMINIMAL_STACK_SIZE * 2, /* Stack size in words, not bytes. */
NULL, /* Parameter passed into the task. */
tskIDLE_PRIORITY + 1, /* Priority at which the task is created. */
NULL, /* Used to pass out the created task's handle. */
0); /* Core ID */
}

Output

Time : 37207    Slope : 3       Raw Value : 273
Fresh air.
Time : 38217 Slope : 3 Raw Value : 269
Fresh air.
Time : 39227 Slope : 3 Raw Value : 274
Fresh air.
Time : 40237 Slope : 3 Raw Value : 251
Fresh air.
Time : 41247 Slope : 3 Raw Value : 276
Fresh air.
Time : 42257 Slope : 3 Raw Value : 250
Fresh air.
Time : 43267 Slope : 3 Raw Value : 236
Fresh air.
Time : 44277 Slope : 3 Raw Value : 253
Fresh air.
Time : 45287 Slope : 3 Raw Value : 245
Fresh air.
Time : 46297 Slope : 3 Raw Value : 249
Fresh air.
Time : 47307 Slope : 3 Raw Value : 244
Fresh air.
Time : 48317 Slope : 3 Raw Value : 235
Fresh air.
Time : 49327 Slope : 3 Raw Value : 239
Fresh air.
Time : 50337 Slope : 3 Raw Value : 233
Fresh air.
Time : 51347 Slope : 3 Raw Value : 235
Fresh air.

Camera and SdCard usage in FreeRTOS

For this I am using the onBoard Camera and SdCard along with ESP_IDF_v5.3.

Hardware Setup

Follow the microSD card guide and camera guide to attach the camera and microSD card extension board to the

  • Format microSD card (supported up to 32Gb)
  • Attach the microSD card to the extension board

The setup would look something like this :

FrontBack

Software Setup

After pulling the git repository, open the folder in VSCode. Go to View->Command Palette->ESP-IDF: Add vscode Configuration Folder. From the bottom panel select the correct COM port, chip (ESP-S3) and build,flash and monitor.

tip

If you are using the OV3660 model, you need to set it up in the IDF to be able to drive it. input "idf.py menuconfig" in your terminal

Step 1Step 2Step 3

Camera Component

  • Camera Configuration:
    • Defines the GPIO pins used for various camera functions (PWDN, RESET, XCLK, SIOD, SIOC, Y9-Y2, VSYNC, HREF, PCLK, LED).
    • Sets default values for camera parameters (e.g., clock frequency, frame buffer location, pixel format, frame size, JPEG quality, frame buffer count, grab mode).
#ifndef CAMERA_CONFIG_H
#define CAMERA_CONFIG_H

#define PWDN_GPIO_NUM -1
#define RESET_GPIO_NUM -1
#define XCLK_GPIO_NUM 10
#define SIOD_GPIO_NUM 40
#define SIOC_GPIO_NUM 39

#define Y9_GPIO_NUM 48
#define Y8_GPIO_NUM 11
#define Y7_GPIO_NUM 12
#define Y6_GPIO_NUM 14
#define Y5_GPIO_NUM 16
#define Y4_GPIO_NUM 18
#define Y3_GPIO_NUM 17
#define Y2_GPIO_NUM 15
#define VSYNC_GPIO_NUM 38
#define HREF_GPIO_NUM 47
#define PCLK_GPIO_NUM 13

#define LED_GPIO_NUM 21

#endif //CAMERA_CONFIG_H
  • Camera Interface:
    Declares functions initialize_camera() and createCameraTask().

  • Camera Implementation:

    • Initializes the camera using the defined configuration.
    void initialize_camera(void)
    {
    camera_config_t camera_config = {
    .pin_pwdn = PWDN_GPIO_NUM,
    .pin_reset = RESET_GPIO_NUM,
    .pin_xclk = XCLK_GPIO_NUM,
    .pin_sccb_sda = SIOD_GPIO_NUM,
    .pin_sccb_scl = SIOC_GPIO_NUM,
    .pin_d7 = Y9_GPIO_NUM,
    .pin_d6 = Y8_GPIO_NUM,
    .pin_d5 = Y7_GPIO_NUM,
    .pin_d4 = Y6_GPIO_NUM,
    .pin_d3 = Y5_GPIO_NUM,
    .pin_d2 = Y4_GPIO_NUM,
    .pin_d1 = Y3_GPIO_NUM,
    .pin_d0 = Y2_GPIO_NUM,
    .pin_vsync = VSYNC_GPIO_NUM,
    .pin_href = HREF_GPIO_NUM,
    .pin_pclk = PCLK_GPIO_NUM,

    .xclk_freq_hz = 20000000, // The clock frequency of the image sensor
    .fb_location = CAMERA_FB_IN_PSRAM, // Set the frame buffer storage location
    .pixel_format = PIXFORMAT_JPEG, // The pixel format of the image: PIXFORMAT_ + YUV422|GRAYSCALE|RGB565|JPEG
    .frame_size = FRAMESIZE_UXGA, // The resolution size of the image: FRAMESIZE_ + QVGA|CIF|VGA|SVGA|XGA|SXGA|UXGA
    .jpeg_quality = 15, // The quality of the JPEG image, ranging from 0 to 63.
    .fb_count = 2, // The number of frame buffers to use.
    .grab_mode = CAMERA_GRAB_LATEST // The image capture mode.
    };

    esp_err_t ret = esp_camera_init(&camera_config);
    if (ret == ESP_OK)
    {
    ESP_LOGI(cameraTag, "Camera configured successful");
    }
    else
    {
    ESP_LOGI(cameraTag, "Camera configured unsuccessful");
    return;
    }
    }
    • Sets camera parameters (brightness, contrast, saturation, special effect, white balance, exposure control, AEC, AE level, AEC value, gain control, AGC gain, gain ceiling, BPC, WPC, raw GMA, LENC, hmirror, vflip, DCW, colorbar).
    sensor_t *s = esp_camera_sensor_get();

    s->set_brightness(s, 0); // -2 to 2
    s->set_contrast(s, 0); // -2 to 2
    s->set_saturation(s, 0); // -2 to 2
    s->set_special_effect(s, 0); // 0 to 6 (0 - No Effect, 1 - Negative, 2 - Grayscale, 3 - Red Tint, 4 - Green Tint, 5 - Blue Tint, 6 - Sepia)
    s->set_whitebal(s, 1); // 0 = disable , 1 = enable
    s->set_awb_gain(s, 1); // 0 = disable , 1 = enable
    s->set_wb_mode(s, 0); // 0 to 4 - if awb_gain enabled (0 - Auto, 1 - Sunny, 2 - Cloudy, 3 - Office, 4 - Home)
    s->set_exposure_ctrl(s, 1); // 0 = disable , 1 = enable
    s->set_aec2(s, 0); // 0 = disable , 1 = enable
    s->set_ae_level(s, 0); // -2 to 2
    s->set_aec_value(s, 300); // 0 to 1200
    s->set_gain_ctrl(s, 1); // 0 = disable , 1 = enable
    s->set_agc_gain(s, 0); // 0 to 30
    s->set_gainceiling(s, (gainceiling_t)0); // 0 to 6
    s->set_bpc(s, 0); // 0 = disable , 1 = enable
    s->set_wpc(s, 1); // 0 = disable , 1 = enable
    s->set_raw_gma(s, 1); // 0 = disable , 1 = enable
    s->set_lenc(s, 1); // 0 = disable , 1 = enable
    s->set_hmirror(s, 0); // 0 = disable , 1 = enable
    s->set_vflip(s, 0); // 0 = disable , 1 = enable
    s->set_dcw(s, 1); // 0 = disable , 1 = enable
    s->set_colorbar(s, 0); // 0 = disable , 1 = enable
    • Defines a function takePicture() to capture an image and save it to SD card.
    void takePicture()
    {
    ESP_LOGI(cameraTag, "Taking picture...");
    camera_fb_t *pic = esp_camera_fb_get();

    if (pic)
    {
    saveJpegToSdcard(pic);
    }

    ESP_LOGI(cameraTag, "Picture taken! Its size was: %zu bytes", pic->len);

    esp_camera_fb_return(pic);
    }
    • Creates a task cameraTakePicture_5_sec() to continuously take pictures every 5 seconds.
    void cameraTakePicture_5_sec(void *pvParameters)
    {
    for (;;)
    {
    takePicture();
    vTaskDelay(5000 / portTICK_PERIOD_MS);
    }
    }

    void createCameraTask()
    {
    TaskHandle_t task;
    xTaskCreate(
    cameraTakePicture_5_sec, /* Function that implements the task. */
    "cameraTakePicture_5_sec", /* Text name for the task. */
    configMINIMAL_STACK_SIZE * 4, /* Stack size in words, or bytes. */
    NULL, /* Parameter passed into the task. */
    tskIDLE_PRIORITY, /* Priority at which the task is created. */
    &task /* Used to pass out the created task's handle. */
    );
    }

Code Structure:

  • Header files (camera_config.h, camera_interface.h) and implementation files (camera_interface.c).
  • The camera_config.h file defines the camera configuration parameters.
  • The camera_interface.h file declares the functions for camera initialization and task creation.
  • The camera_interface.c file implements the camera initialization, picture-taking, and task creation logic.

SdCard Component

  • SD Card Configuration:
    Defines the GPIO pins used for the SD card interface (MISO, MOSI, CLK, CS).
#ifndef SDCARD_CONFIG_H
#define SDCARD_CONFIG_H

#define PIN_NUM_MISO GPIO_NUM_8
#define PIN_NUM_MOSI GPIO_NUM_9
#define PIN_NUM_CLK GPIO_NUM_7
#define PIN_NUM_CS GPIO_NUM_21

#endif //SDCARD_CONFIG_H
  • SD Card Interface:
    Declares functions initialize_sdcard(), deinitialize_sdcard(), and saveJpegToSdcard().
#ifndef SDCARD_INTERFACE_H
#define SDCARD_INTERFACE_H

#include "esp_camera.h"

void initialize_sdcard(void);
void deinitialize_sdcard();
void saveJpegToSdcard(camera_fb_t *);

#endif //SDCARD_INTERFACE_H
  • SD Card Implementation:

    • Initializes the SD card using the defined configuration and mounts the SD card as a FAT filesystem.
    sdmmc_card_t *card;
    sdmmc_host_t host = SDSPI_HOST_DEFAULT();
    const char mount_point[] = "/sd";

    void initialize_sdcard()
    {
    esp_err_t ret;

    // If format_if_mount_failed is set to true, SD card will be partitioned and
    // formatted in case when mounting fails.
    esp_vfs_fat_sdmmc_mount_config_t mount_config = {
    #ifdef FORMAT_IF_MOUNT_FAILED
    .format_if_mount_failed = true,
    #else
    .format_if_mount_failed = false,
    #endif // EXAMPLE_FORMAT_IF_MOUNT_FAILED
    .max_files = 5,
    .allocation_unit_size = 32 * 1024};

    ESP_LOGI(sdcardTag, "Initializing SD card");

    // Use settings defined above to initialize SD card and mount FAT filesystem.
    // Note: esp_vfs_fat_sdmmc/sdspi_mount is all-in-one convenience functions.
    // Please check its source code and implement error recovery when developing
    // production applications.
    ESP_LOGI(sdcardTag, "Using SPI peripheral");

    // By default, SD card frequency is initialized to SDMMC_FREQ_DEFAULT (20MHz)
    // For setting a specific frequency, use host.max_freq_khz (range 400kHz - 20MHz for SDSPI)
    spi_bus_config_t bus_cfg = {
    .mosi_io_num = PIN_NUM_MOSI,
    .miso_io_num = PIN_NUM_MISO,
    .sclk_io_num = PIN_NUM_CLK,
    .quadwp_io_num = -1,
    .quadhd_io_num = -1,
    .max_transfer_sz = host.max_freq_khz,
    };
    ret = spi_bus_initialize(host.slot, &bus_cfg, SDSPI_DEFAULT_DMA);
    if (ret != ESP_OK)
    {
    ESP_LOGE(sdcardTag, "Failed to initialize bus.");
    return;
    }

    // This initializes the slot without card detect (CD) and write protect (WP) signals.
    // Modify slot_config.gpio_cd and slot_config.gpio_wp if your board has these signals.
    sdspi_device_config_t slot_config = SDSPI_DEVICE_CONFIG_DEFAULT();
    slot_config.gpio_cs = PIN_NUM_CS;
    slot_config.host_id = host.slot;

    ESP_LOGI(sdcardTag, "Mounting filesystem");
    ret = esp_vfs_fat_sdspi_mount(mount_point, &host, &slot_config, &mount_config, &card);

    if (ret != ESP_OK)
    {
    if (ret == ESP_FAIL)
    {
    ESP_LOGE(sdcardTag, "Failed to mount filesystem. "
    "If you want the card to be formatted, set the FORMAT_IF_MOUNT_FAILED in sdcard_config.h");
    }
    else
    {
    ESP_LOGE(sdcardTag, "Failed to initialize the card (%s). "
    "Make sure SD card lines have pull-up resistors in place.",
    esp_err_to_name(ret));
    }
    return;
    }
    ESP_LOGI(sdcardTag, "Filesystem mounted");

    // Card has been initialized, print its properties
    sdmmc_card_print_info(stdout, card);

    // Format FATFS
    #ifdef FORMAT_SD_CARD
    ret = esp_vfs_fat_sdcard_format(mount_point, card);
    if (ret != ESP_OK)
    {
    ESP_LOGE(sdcardTag, "Failed to format FATFS (%s)", esp_err_to_name(ret));
    return;
    }

    if (stat(file_foo, &st) == 0)
    {
    ESP_LOGI(sdcardTag, "file still exists");
    return;
    }
    else
    {
    ESP_LOGI(sdcardTag, "file doesnt exist, format done");
    }
    #endif // CONFIG_EXAMPLE_FORMAT_SD_CARD
    }
    • Provides functions to save JPEG images to the SD card.
    uint16_t lastKnownFile = 0;

    void saveJpegToSdcard(camera_fb_t *captureImage)
    {
    // Find the next available filename
    char filename[32];

    sprintf(filename, "%s/%u_img.jpg", mount_point, lastKnownFile++);

    // Create the file and write the JPEG data
    FILE *fp = fopen(filename, "wb");
    if (fp != NULL)
    {
    fwrite(captureImage->buf, 1, captureImage->len, fp);
    fclose(fp);
    ESP_LOGI(sdcardTag, "JPEG saved as %s", filename);
    }
    else
    {
    ESP_LOGE(sdcardTag, "Failed to create file: %s", filename);
    }
    }

Component Structure:

  • Header files (sdcard_config.h, sdcard_interface.h) and implementation files (sdcard_interface.c).
  • The sdcard_config.h file defines the SD card configuration parameters.
  • The sdcard_interface.h file declares the functions for SD card initialization, deinitialization, and image saving.
  • The sdcard_interface.c file implements the SD card initialization, deinitialization, and image saving logic.

Main Function

// main.c
#include <stdio.h>
#include "camera_interface.h"
#include "sdcard_interface.h"

void initialize_drivers()
{
initialize_sdcard();
initialize_camera();
}

void start_tasks()
{
createCameraTask();
}

void app_main(void)
{
initialize_drivers();
start_tasks();
}
  • Includes necessary header files for camera and SD card interfaces.
  • Initializes both the SD card and camera using the provided functions.
  • Starts the camera task to continuously take pictures

Output

pir

UART Output

I (1119) main_task: Calling app_main()
I (1123) sdcard: Initializing SD card
I (1127) sdcard: Using SPI peripheral
I (1132) sdcard: Mounting filesystem
I (1137) gpio: GPIO[21]| InputEn: 0| OutputEn: 1| OpenDrain: 0| Pullup: 0| Pulldown: 0| Intr:0
I (1146) sdspi_transaction: cmd=52, R1 response: command not supported
I (1195) sdspi_transaction: cmd=5, R1 response: command not supported
I (1219) sdcard: Filesystem mounted
Name: SD32G
Type: SDHC/SDXC
Speed: 20.00 MHz (limit: 20.00 MHz)
Size: 30448MB
CSD: ver=2, sector_size=512, capacity=62357504 read_bl_len=9
SSR: bus_width=1
I (1226) s3 ll_cam: DMA Channel=1
I (1230) cam_hal: cam init ok
I (1234) sccb: pin_sda 40 pin_scl 39
I (1238) sccb: sccb_i2c_port=1
I (1252) camera: Detected camera at address=0x30
I (1255) camera: Detected OV2640 camera
I (1255) camera: Camera PID=0x26 VER=0x42 MIDL=0x7f MIDH=0xa2
I (1344) cam_hal: buffer_size: 16384, half_buffer_size: 1024, node_buffer_size: 1024, node_cnt: 16, total_cnt: 375
I (1344) cam_hal: Allocating 384000 Byte frame buffer in PSRAM
I (1351) cam_hal: Allocating 384000 Byte frame buffer in PSRAM
I (1357) cam_hal: cam config ok
I (1361) ov2640: Set PLL: clk_2x: 0, clk_div: 0, pclk_auto: 0, pclk_div: 12
I (1453) camera: Camera configured successful
I (1487) main_task: Returned from app_main()
I (1487) camera: Taking picture...
I (1997) sdcard: JPEG saved as /sd/0_img.jpg
I (1997) camera: Picture taken! Its size was: 45764 bytes
I (6997) camera: Taking picture...
I (7348) sdcard: JPEG saved as /sd/1_img.jpg
I (7349) camera: Picture taken! Its size was: 51710 bytes
I (12349) camera: Taking picture...
I (12704) sdcard: JPEG saved as /sd/2_img.jpg
I (12705) camera: Picture taken! Its size was: 51853 bytes
I (17706) camera: Taking picture...
I (18054) sdcard: JPEG saved as /sd/3_img.jpg
I (18055) camera: Picture taken! Its size was: 51919 bytes
I (23055) camera: Taking picture...
I (23414) sdcard: JPEG saved as /sd/4_img.jpg
I (23414) camera: Picture taken! Its size was: 51809 bytes
I (28415) camera: Taking picture...
I (28768) sdcard: JPEG saved as /sd/5_img.jpg
I (28768) camera: Picture taken! Its size was: 51747 bytes
I (33771) camera: Taking picture...
I (34117) sdcard: JPEG saved as /sd/6_img.jpg
I (34117) camera: Picture taken! Its size was: 51968 bytes

Output Image

pir

FreeRtos for Arduino IDE

FreeRtos can be used for Arduino-IDE based XIAO-S3 builds. It is similar to ESP-IDF usable but it runs on only one core and is not optimized for ESP-IDF.

Hardware Setup

Attach the Xiao-S3 to the Grove - Expansion Board (OLED DIsplay and RTC) and connect the Grove - Temperature, Humidity, Pressure and Gas Sensor for Arduino - BME680 to the I2c Bus.

pir

Software Setup

Install the arduino libraries for pcf8563, U8x8lib and bme680 library. Refer to How to install library to install library for Arduino.

#include "time.h"
#include <WiFi.h>
#include <PCF8563.h>
#include <U8x8lib.h>
#include <Wire.h>
#include "seeed_bme680.h"

#define IIC_ADDR uint8_t(0x76)
Seeed_BME680 bme680(IIC_ADDR); /* IIC PROTOCOL */

// I2C communication library for the PCF8563 real-time clock
PCF8563 pcf;

// OLED display library
U8X8_SSD1306_128X64_NONAME_HW_I2C u8x8(/* clock=*/D4, /* data=*/D5, /* reset=*/U8X8_PIN_NONE); // OLEDs without Reset of the Display

// WiFi network credentials
const char* ssid = "REPLACE_WITH_YOUR_SSID";
const char* password = "REPLACE_WITH_YOUR_PASSWORD";

// NTP server for time synchronization
const char* ntpServer = "pool.ntp.org";

// Timezone offset (adjust based on your location)
const long gmtOffset_sec = 5.5 * 60 * 60; // Hours * Minutes * Seconds (here, GMT+5:30)
const int daylightOffset_sec = 0; // No daylight saving time assumed

// Global variable to store current time information
static Time nowTime;

// Function prototypes for tasks
void printDateAndTime(void* pvParameters);
void updateTime(void* pvParameters);
void ledBlink2Hz(void* pvParameters);
void oledDisplayUpdate(void* pvParameters);
void taskBME680(void* pvParameters);

// Setup function (runs once at startup)
void setup() {

Serial.begin(115200); // Initialize serial communication for debugging

// Set built-in LED pin as output for blinking
pinMode(LED_BUILTIN, OUTPUT);

Serial.print("Connecting to ");
Serial.println(ssid);
WiFi.begin(ssid, password); // Connect to WiFi network
while (WiFi.status() != WL_CONNECTED) {
delay(500);
Serial.print(".");
}

while (!bme680.init()) {
Serial.println("bme680 init failed ! can't find device!");
delay(10000);
}

pcf.init(); // Initialize the PCF8563 real-time clock

// Stop the clock before setting the time
pcf.stopClock();

// Configure time synchronization using NTP server
configTime(gmtOffset_sec, daylightOffset_sec, ntpServer);
static struct tm timeinfo;
while (!getLocalTime(&timeinfo)) {
Serial.println("no received time info ... Waiting ...");
}

// Set the time on the PCF8563 clock based on retrieved time
pcf.setYear(timeinfo.tm_year);
pcf.setMonth(timeinfo.tm_mon);
pcf.setDay(timeinfo.tm_mday);
pcf.setHour(timeinfo.tm_hour);
pcf.setMinut(timeinfo.tm_min);
pcf.setSecond(timeinfo.tm_sec);

pcf.startClock(); // Start the clock after setting the time

Serial.println("WiFi connected at " + WiFi.localIP());

u8x8.begin(); // Initialize the OLED display
u8x8.setFlipMode(1); // Optionally rotate OLED display content

// Create tasks for different functionalities
xTaskCreate(
updateTime,
"Get LocalTime",
configMINIMAL_STACK_SIZE * 2,
(void*)1,
tskIDLE_PRIORITY + 1,
NULL);

xTaskCreate(
ledBlink2Hz,
"Task 2",
configMINIMAL_STACK_SIZE,
(void*)1,
tskIDLE_PRIORITY + 1,
NULL);

xTaskCreate(
oledDisplayUpdate,
"OLED Display Task",
configMINIMAL_STACK_SIZE * 2,
(void*)1,
tskIDLE_PRIORITY,
NULL);

xTaskCreate(
printDateAndTime,
"Print Uart",
configMINIMAL_STACK_SIZE * 2,
(void*)1,
tskIDLE_PRIORITY,
NULL);

xTaskCreate(
taskBME680,
"BME680 Sensor Poll",
configMINIMAL_STACK_SIZE * 2,
(void*)1,
tskIDLE_PRIORITY + 1,
NULL);
}

// Loop function (doesn't do anything in this case, tasks handle everything)
void loop() {
// Nothing to do here, all work is done in the tasks
}

// Function that will run as a task: Prints current date and time to serial port
void printDateAndTime(void* pvParameters) {
for (;;) {
// Print current time in formatted string (DD/MM/YY\tHH:MM:SS) to serial port
Serial.printf("%02d/%02d/%02d\t%02d:%02d:%02d\n",
nowTime.day, nowTime.month + 1, nowTime.year % 100,
nowTime.hour, nowTime.minute, nowTime.second);
// Delay for 1 second before reading time again
vTaskDelay(1000 / portTICK_PERIOD_MS);
}
}

// Function that will run as a task: Reads current time from PCF8563 clock
void updateTime(void* pvParameters) {
for (;;) {
// Update the global `nowTime` variable with the current time from the PCF8563 clock
nowTime = pcf.getTime();
// Delay for 0.5 second before reading time again (can be adjusted for desired update frequency)
vTaskDelay(500 / portTICK_PERIOD_MS);
}
}

// Function that will run as a task: Blinks the built-in LED at 2Hz
void ledBlink2Hz(void* pvParameters) {
bool state = true; // Initial state for LED (on or off)
for (;;) {
// Set LED state (HIGH for on, LOW for off)
digitalWrite(LED_BUILTIN, (state ? HIGH : LOW));
// Delay for 0.5 second to create a 2Hz blinking frequency (one cycle on/off)
vTaskDelay(500 / portTICK_PERIOD_MS);
// Toggle LED state for the next cycle
state = !state;
}
}

// Function that will run as a task: Updates OLED display with date and time
void oledDisplayUpdate(void* pvParameters) {
for (;;) {

// Set font for the first line (date)
u8x8.setFont(u8x8_font_chroma48medium8_r);

// Set cursor position for the first line (centered)
u8x8.setCursor(0, 0);

char buffer1[12]; // Buffer to hold formatted date string
std::snprintf(buffer1, sizeof(buffer1), "%02d/%02d/%02d",
nowTime.day, nowTime.month + 1, nowTime.year % 100);
u8x8.print(buffer1);

// Format time string (HH:MM:SS) into buffer2 using std::snprintf
std::snprintf(buffer1, sizeof(buffer1), "%02d:%02d:%02d",
nowTime.hour, nowTime.minute, nowTime.second);
// Print formatted time string to OLED display
u8x8.print(buffer1);

// Adjust cursor position for the second line (below the first line)
u8x8.setCursor(0, 10);

char buffer2[20]; // Buffer to hold formatted sensor data

std::snprintf(buffer2, sizeof(buffer2), "T: %.1f°C", bme680.sensor_result_value.temperature);
u8x8.print(buffer2);
u8x8.setCursor(0, 20);

std::snprintf(buffer2, sizeof(buffer2), "P: %.1fkPa", bme680.sensor_result_value.pressure / 1000.0);
u8x8.print(buffer2);

u8x8.setCursor(0, 30);

std::snprintf(buffer2, sizeof(buffer2), "H: %.1f%%", bme680.sensor_result_value.humidity);
u8x8.print(buffer2);

// std::snprintf(buffer2, sizeof(buffer2), "G: %.1f Kohms", bme680.sensor_result_value.gas / 1000.0);
// u8x8.print(buffer2);

vTaskDelay(100 / portTICK_PERIOD_MS); // Update every 0.1 seconds (adjust as needed)
}
}

void taskBME680(void* pvParameters) {
for (;;) {
if (bme680.read_sensor_data()) {
Serial.println("Failed to perform reading :(");
} else {
Serial.print("T: ");
Serial.print(bme680.sensor_result_value.temperature, 2);
Serial.print(" C P: ");
Serial.print(bme680.sensor_result_value.pressure / 1000.0, 2);
Serial.print(" KPa H: ");
Serial.print(bme680.sensor_result_value.humidity, 2);
Serial.print(" % G: ");
Serial.print(bme680.sensor_result_value.gas / 1000.0, 2);
Serial.println(" Kohms");
}

vTaskDelay(1000 / portTICK_PERIOD_MS);
}
}

Output

pir

Serial Monitor Output

09/09/24 03:17:20
T: 29.01 C P: 90.86 KPa H: 63.41 % G: 47.41 Kohms
09/09/24 03:17:21
T: 29.03 C P: 90.86 KPa H: 63.34 % G: 47.85 Kohms

Arduino FreeRtos vs ESP-IDF FreeRtos

FeatureArduino FreeRTOSESP-IDF FreeRTOS
Abstraction LayerHigher-level abstraction, easier for beginnersLower-level abstraction, more control for experienced users
Development EnvironmentArduino IDEESP-IDF command-line tools
CompatibilityPrimarily compatible with Arduino-based boardsCompatible with a wider range of ESP32 and ESP32-S2 boards
FeaturesBasic RTOS features, task creation, scheduling, synchronizationComprehensive RTOS features, task creation, scheduling, synchronization, event groups, queues, mutexes, semaphores
PerformanceGenerally less performant due to the abstraction layerMore performant due to direct access to hardware and RTOS APIs
CustomizationLimited customization optionsExtensive customization options through configuration files and APIs
Learning CurveEasier to learn for beginnersSteeper learning curve for those unfamiliar with command-line tools and C/C++
Use CasesSimple IoT projects, prototypingComplex IoT applications, real-time systems, custom hardware

Trouble Shooting

Some problems might encounter in the process of hardware connection, software debugging or uploading.

Tech Support & Product Discussion

Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.

Loading Comments...